I2C Multi master support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Multi master support

2,371 Views
NithinkumarN
Contributor II

Hi All,

I'm working on i.MX6Q processor custom board.

I will use L3.0.35_4.1.0 freescale release code.

I need to test I2C multi master in my platform.

Please let me know , this feature is already present in existing I2C driver of L3.0.35_4.1.0 release linux kernel.

Thanks and Regards,

Nithin

Labels (2)
0 Kudos
Reply
2 Replies

2,066 Views
art
NXP Employee
NXP Employee

The only feature of the L3.0.35 BSP I2C driver that can help to support the multi-master I2C bus is the possibility to generate the Arbitration Lost interrupt in case of losing bus arbitration during the master data transfer. No other features are provided.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,066 Views
NithinkumarN
Contributor II

Hi All,

Any update on above query, Please let me know as soon as possible since I'm in implementation stage.

Thanks and Regards,

Nithin

0 Kudos
Reply