I210 performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I210 performance

1,729 次查看
damienhuang
Contributor IV

Hi,

I added the intel i210 ethernet chip to the sabrelite board and recompiled the boundary lollipop 5.0.0 kernel with

CONFIG_NET_VENDOR_INTEL=y

CONFIG_IGB=y
CONFIG_IGB_HWMON=y

but when I test it with 'iperf' command, the result is far slower from Gigabit (see below for results)

Testing with 480M ... result: 62.9 Mbits/sec
Testing with 400M ... result: 66.3 Mbits/sec
Testing with 300M ... result: 156 Mbits/sec
Testing with 200M ... result: 199 Mbits/sec
Testing with 100M ... result: 100 Mbits/sec

has anyone tested this chip on the lollipop kernel and can get better result? or anyone knows how to improve the result?

Cheers,

Damien

0 项奖励
回复
1 回复

1,414 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Damien

please check

i.MX6 Gigabit Ethernet - Boundary Devices 

About Gigabit Ethernet performance gap between Android&Linux 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复