I210 performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I210 performance

2,353件の閲覧回数
damienhuang
Contributor IV

Hi,

I added the intel i210 ethernet chip to the sabrelite board and recompiled the boundary lollipop 5.0.0 kernel with

CONFIG_NET_VENDOR_INTEL=y

CONFIG_IGB=y
CONFIG_IGB_HWMON=y

but when I test it with 'iperf' command, the result is far slower from Gigabit (see below for results)

Testing with 480M ... result: 62.9 Mbits/sec
Testing with 400M ... result: 66.3 Mbits/sec
Testing with 300M ... result: 156 Mbits/sec
Testing with 200M ... result: 199 Mbits/sec
Testing with 100M ... result: 100 Mbits/sec

has anyone tested this chip on the lollipop kernel and can get better result? or anyone knows how to improve the result?

Cheers,

Damien

0 件の賞賛
返信
1 返信

2,038件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Damien

please check

i.MX6 Gigabit Ethernet - Boundary Devices 

About Gigabit Ethernet performance gap between Android&Linux 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信