I

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,719件の閲覧回数
cyrusvali
Contributor II

Hi

I have a question about ARM architecture

why there is two registers to enable/disable interrupts? ISER and ICER

Is it not possible to set/reset the same register for enable/disabling the interrupts?

thank you

1 解決策
1,612件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,613件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------