I need WinCE patch to support BT656 and BT1120 Output For i.MX515 BSP ,who can help me ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need WinCE patch to support BT656 and BT1120 Output For i.MX515 BSP ,who can help me ?

ソリューションへジャンプ
2,210件の閲覧回数
36766362
Contributor I

I need wince patch to support BT656 and BT1120 Output For i.MX515 BSP  ,who can help me ?

ラベル(4)
0 件の賞賛
返信
1 解決策
1,880件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,881件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,881件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ming,

The maximal input clock supported by the vide CSI in i.MX51 is 120 MHz.

The limit of 45 MP/sec assumes:

-          2 bus cycles per pixel; e.g. BT.656

-          35% blanking overhead.


The standard pixel clock rate for 1280x720 @ 60 fps is 75 MHz, so the CSI supports this rate with BT.1120 (10+10-bit bus; 1 bus cycle per pixel), but not with BT.656.

1280x720 @ 60 fps could be possible with BT.656 only if the blanking overhead can be reduced below ~8.5% (~120M / (1280x720x60x2) )

In case of BT1120 Any scaling operation of PSF or Interlaced image would require first converting the image to Progressive format, prior to scaling. So I’m not sure that I clearly understand your use case.

Note that our Linux or WinCE BSP software packages may not include support for some unusual cases. The answers here are related to hardware capabilities only.

"By default, camera driver for i.MX51 Windows CE BSP can not support interlaced CSI input. Please do following changes to the camera driver to support interlaced CSI input:


1) open    filewince600\platform\imx51-3ds\files\platform.reg, for the registry item "[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Camera]", field ""CameraId", change the CameraId from 0 to 4 or 5. Value 4 or 5 to CameraId means interlaced CSI input.

2) Open file wince600\platform\common\src\soc\common_fsl_v2\ipuv3\camera\pdd\sensorpdd.cpp, go to function ReadCSIInterfaceFromRegistry(), note the following segment of code: case 4: case 5: //reserved for TVin support


#if 0 //Tvin maybe interlace mode or progressive mode m_PrtclInf.mode = CSI_CCIR_PROGRESSIVE_BT656_MODE, m_PrtclInf.mode = CSI_CCIR_INTERLACE_BT656_MODE; // Set the following parameters due to the interlace or progressive mode m_PrtclInf.PreCmd; m_PrtclInf.Field0FirstBlankStartCmd; m_PrtclInf.Field0FirstBlankEndCmd; m_PrtclInf.Field0SecondBlankStartCmd; m_PrtclInf.Field0SecondBlankEndCmd; m_PrtclInf.Field0ActiveStartCmd; m_PrtclInf.Field0ActiveEndCmd; #endif m_bCsiTstMode = FALSE; break; The code segment between "#if 0" and "#endif" is reserved for interlaced mode CSI input. Please enable this code segment to enable interlaced mode support ----- that means, customer should change "#if 0" to

"#if 1" and set the value of parameters: m_PrtclInf.Field0FirstBlankStartCmd, m_PrtclInf.Field0FirstBlankEndCmd, m_PrtclInf.Field0SecondBlankStartCmd, m_PrtclInf.Field0SecondBlankEndCmd,m_PrtclInf.Field0ActiveStartCmd,m_PrtclInf.Field0ActiveEndCmd according to their camera type."

Unfortunately there is no any patch for wince with the implementaton.

Hope this helps

1,881件の閲覧回数
36766362
Contributor I

Hi  Bio_TICFSL:

     Thanks for your answer.But I need WinCE patch For i.MX515  to support BT656 or BT1120 Output on DI0  or DI1 , not on CSI .

0 件の賞賛
返信
1,881件の閲覧回数
art
NXP Employee
NXP Employee

There is no ready to use patch from Freescale to support BT656 or BT1120 display output on i.MX51 processors.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信