I.mx6ul interface with SI3050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.mx6ul interface with SI3050

2,311 次查看
maheshk
Contributor II

Hi All

can anybody please explain how  SI3050 Voice DAA https://www.silabs.com/Support%20Documents/TechnicalDocs/Si3050-11-18-19.pdf can be interfaced to I.MX6 UL ?

As SI3050 has SPI & PCM highway data interface for control as well as Data .

Thanks in advance

Mahesh k

标签 (1)
0 项奖励
回复
3 回复数

2,102 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

seems it can be connected to SAI on TDM/I2S mode according to

Table 21 (PCM mode), for SAI usage one can look at

http://cache.freescale.com/files/microcontrollers/doc/AN4486.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,102 次查看
maheshk
Contributor II

Hi Igor,

Thanks for the reply. I have one more query to you. can you please

send the link to download IOMUX tool particularly for I.MX6UL. The

tool one I have supports I.mx6 series processors except Ultralite. so

kindly give a solution.

Thanks

Mahesh k

Quoting igorpadykov <[email protected]>:

igorpadykov

replied to the discussion

"I.mx6ul interface with SI3050"

To view the discussion, visit:

https://community.freescale.com/message/614381?et=watches.email.thread#614381

>

0 项奖励
回复

2,102 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

please use Processor Expert instead IOMUX tool

Processor Expert for i.MX|NXP

~igor

0 项奖励
回复