I have on i.mx6 dual question too~
~# echo g > /proc/sysrq-trigger work good
but Kgdbwait into wait state, but GDB can not connect
of course I exit the mincom~ also try to use
git://git.kernel.org/pub/scm/utils/kernel/kgdb/agent-proxy.git
still can not work
/////gdb message
174,060 &"symbol-file /root/project_board/free_imx/out/matrix_io/kernel/vmlinux\n"
174,060 ~"Reading symbols from /root/project_board/free_imx/out/matrix_io/kernel/vmlinux..."
174,118 12-list-thread-groups
175,042 ~"done.\n"
175,044 11^done
175,044 (gdb)
175,044 &"\n"
175,045 ^done
175,045 (gdb)
175,045 12^done,groups=[{id="i1",type="process"}]
175,045 (gdb)
175,046 13-target-select remote /dev/ttyUSB0
196,053 ~"Ignoring packet error, continuing...\n"
196,053 &"warning: unrecognized item \"timeout\" in \"qSupported\" response\n"
/////bootargs message
boot
booti mmc1
kernel @ 14008000 (9372264)
ramdisk @ 15000000 (507162)
fdt @ 14f00000 (55103)
kernel cmdline:
use boot.img command line:
kgdboc=ttymxc0,115200 kgdbwait init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2
ff video=mxcfb3
ff vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M mem=1G
switch to ldo_bypass mode!
Using Device Tree in place at 14f00000, end 14f1073e
Starting kernel ...
/////kernel boot message
2.336547] calling sched_clock_syscore_init+0x0/0x24 @ 1
[ 2.336580] initcall sched_clock_syscore_init+0x0/0x24 returned 0 after 2 usecs
[ 2.336596] Doing 0
[ 2.336623] calling register_pmu_driver+0x0/0x6c @ 1
[ 2.336974] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[ 2.338491] initcall register_pmu_driver+0x0/0x6c returned 0 after 1789 usecs
[ 2.338512] Doing 1
[ 2.338542] calling mxc_epit_driver_init+0x0/0x24 @ 1
[ 2.339437] initcall mxc_epit_driver_init+0x0/0x24 returned 0 after 843 usecs
[ 2.339458] Doing 2
[ 2.339485] calling ldo2p5_dummy_driver_init+0x0/0x24 @ 1
[ 2.340766] initcall ldo2p5_dummy_driver_init+0x0/0x24 returned 0 after 1222 usecs
[ 2.340786] Doing 3
[ 2.340811] calling busfreq_init+0x0/0x44 @ 1
[ 2.341551] imx6_busfreq busfreq.16: DDR medium rate not supported.
[ 2.342400] Bus freq driver module loaded
[ 2.342437] initcall busfreq_init+0x0/0x44 returned 0 after 1557 usecs
[ 2.342453] Doing 4
[ 2.342479] calling mxc_bt_rfkill_driver_init+0x0/0x24 @ 1
[ 2.342991] initcall mxc_bt_rfkill_driver_init+0x0/0x24 returned 0 after 470 usecs
[ 2.343009] Doing 5
[ 2.343035] calling mx6_ir_driver_init+0x0/0x24 @ 1
[ 2.343503] initcall mx6_ir_driver_init+0x0/0x24 returned 0 after 427 usecs
[ 2.343520] Doing 6
[ 2.343545] calling mxc_ramoops_driver_init+0x0/0x24 @ 1
[ 2.353513] console [pstore-1] enabled
[ 2.353540] ramoops: attached 0x100000@0x4bf00000, ecc: 0/0
[ 2.353578] mxc_ramoops device success loaded
[ 2.353730] initcall mxc_ramoops_driver_init+0x0/0x24 returned 0 after 9909 usecs
[ 2.353752] Doing 7
[ 2.353785] calling proc_execdomains_init+0x0/0x68 @ 1
[ 2.353844] initcall proc_execdomains_init+0x0/0x68 returned 0 after 23 usecs
[ 2.353862] Doing 8
[ 2.353892] calling ioresources_init+0x0/0xb0 @ 1
[ 2.353951] initcall ioresources_init+0x0/0xb0 returned 0 after 26 usecs
[ 2.353971] Doing 9
[ 2.354000] calling uid_cache_init+0x0/0x104 @ 1
[ 2.354063] initcall uid_cache_init+0x0/0x104 returned 0 after 28 usecs
[ 2.354082] Doing 10
[ 2.354114] calling init_posix_timers+0x0/0x538 @ 1
[ 2.354242] initcall init_posix_timers+0x0/0x538 returned 0 after 88 usecs
[ 2.354342] Doing 11
[ 2.354379] calling init_posix_cpu_timers+0x0/0x200 @ 1
[ 2.354418] initcall init_posix_cpu_timers+0x0/0x200 returned 0 after 1 usecs
[ 2.354436] Doing 12
[ 2.354468] calling proc_schedstat_init+0x0/0x68 @ 1
[ 2.354522] initcall proc_schedstat_init+0x0/0x68 returned 0 after 18 usecs
[ 2.354542] Doing 13
[ 2.354573] calling android_power_init+0x0/0x98 @ 1
[ 2.354632] initcall android_power_init+0x0/0x98 returned 0 after 24 usecs
[ 2.354651] Doing 14
[ 2.354684] calling suspend_time_syscore_init+0x0/0x2c @ 1
[ 2.354716] initcall suspend_time_syscore_init+0x0/0x2c returned 0 after 2 usecs
[ 2.354735] Doing 15
[ 2.354765] calling timekeeping_init_ops+0x0/0x24 @ 1
[ 2.354799] initcall timekeeping_init_ops+0x0/0x24 returned 0 after 1 usecs
[ 2.354817] Doing 16
[ 2.354847] calling init_clocksource_sysfs+0x0/0x98 @ 1
[ 2.355254] initcall init_clocksource_sysfs+0x0/0x98 returned 0 after 356 usecs
[ 2.355277] Doing 17
[ 2.355309] calling init_timer_list_procfs+0x0/0x84 @ 1
[ 2.355364] initcall init_timer_list_procfs+0x0/0x84 returned 0 after 15 usecs
[ 2.355385] Doing 18
[ 2.355416] calling alarmtimer_init+0x0/0x380 @ 1
[ 2.356013] initcall alarmtimer_init+0x0/0x380 returned 0 after 541 usecs
[ 2.356037] Doing 19
[ 2.356069] calling init_tstats_procfs+0x0/0x84 @ 1
[ 2.356126] initcall init_tstats_procfs+0x0/0x84 returned 0 after 17 usecs
[ 2.356147] Doing 20
[ 2.356175] calling futex_init+0x0/0x214 @ 1
[ 2.356351] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 2.356441] initcall futex_init+0x0/0x214 returned 0 after 219 usecs
[ 2.356460] Doing 21
[ 2.356489] calling proc_modules_init+0x0/0x68 @ 1
[ 2.356539] initcall proc_modules_init+0x0/0x68 returned 0 after 17 usecs
[ 2.356560] Doing 22
[ 2.356586] calling kallsyms_init+0x0/0x68 @ 1
[ 2.356628] initcall kallsyms_init+0x0/0x68 returned 0 after 13 usecs
[ 2.356650] Doing 23
[ 2.356676] calling audit_init+0x0/0x2ac @ 1
[ 2.356697] audit: initializing netlink socket (disabled)
[ 2.356786] type=2000 audit(2.270:1): initialized
[ 2.356832] initcall audit_init+0x0/0x2ac returned 0 after 120 usecs
[ 2.356850] Doing 24
[ 2.356877] calling audit_watch_init+0x0/0x80 @ 1
[ 2.356913] initcall audit_watch_init+0x0/0x80 returned 0 after 7 usecs
[ 2.356930] Doing 25
[ 2.356955] calling audit_tree_init+0x0/0xc4 @ 1
[ 2.356991] initcall audit_tree_init+0x0/0xc4 returned 0 after 7 usecs
[ 2.357010] Doing 26
[ 2.357035] calling init_kprobes+0x0/0x1cc @ 1
[ 2.794178] initcall init_kprobes+0x0/0x1cc returned 0 after 426854 usecs
[ 2.794209] Doing 27
[ 2.794238] calling irq_gc_init_ops+0x0/0x24 @ 1
[ 2.794321] initcall irq_gc_init_ops+0x0/0x24 returned 0 after 1 usecs
[ 2.794343] Doing 28
[ 2.794370] calling irq_pm_init_ops+0x0/0x24 @ 1
[ 2.794401] initcall irq_pm_init_ops+0x0/0x24 returned 0 after 1 usecs
[ 2.794419] Doing 29
[ 2.794448] calling utsname_sysctl_init+0x0/0x24 @ 1
[ 2.794526] initcall utsname_sysctl_init+0x0/0x24 returned 0 after 45 usecs
[ 2.794547] Doing 30
[ 2.794582] calling init_tracepoints+0x0/0x2c @ 1
[ 2.794615] initcall init_tracepoints+0x0/0x2c returned 0 after 1 usecs
[ 2.794634] Doing 31
[ 2.794661] calling stack_trace_init+0x0/0xf8 @ 1
[ 2.794777] initcall stack_trace_init+0x0/0xf8 returned 0 after 80 usecs
[ 2.794800] Doing 32
[ 2.794832] calling irq_work_init_cpu_notifier+0x0/0x48 @ 1
[ 2.794872] initcall irq_work_init_cpu_notifier+0x0/0x48 returned 0 after 7 usecs
[ 2.794890] Doing 33
[ 2.794917] calling perf_event_sysfs_init+0x0/0x148 @ 1
[ 2.795692] initcall perf_event_sysfs_init+0x0/0x148 returned 0 after 718 usecs
[ 2.795719] Doing 34
[ 2.795752] calling init_per_zone_wmark_min+0x0/0xac @ 1
[ 2.797220] initcall init_per_zone_wmark_min+0x0/0xac returned 0 after 1392 usecs
[ 2.797247] Doing 35
[ 2.797281] calling kswapd_init+0x0/0x58 @ 1
[ 2.797913] initcall kswapd_init+0x0/0x58 returned 0 after 575 usecs
[ 2.797940] Doing 36
[ 2.797970] calling extfrag_debug_init+0x0/0xc4 @ 1
[ 2.798081] initcall extfrag_debug_init+0x0/0xc4 returned 0 after 75 usecs
[ 2.798105] Doing 37
[ 2.798139] calling setup_vmstat+0x0/0x1c8 @ 1
[ 2.798244] initcall setup_vmstat+0x0/0x1c8 returned 0 after 69 usecs
[ 2.798265] Doing 38
[ 2.798293] calling mm_sysfs_init+0x0/0x60 @ 1
[ 2.798352] initcall mm_sysfs_init+0x0/0x60 returned 0 after 26 usecs
[ 2.798372] Doing 39
[ 2.798404] calling init_reserve_notifier+0x0/0x30 @ 1
[ 2.798437] initcall init_reserve_notifier+0x0/0x30 returned 0 after 1 usecs
[ 2.798454] Doing 40
[ 2.798486] calling init_admin_reserve+0x0/0xac @ 1
[ 2.798518] initcall init_admin_reserve+0x0/0xac returned 0 after 2 usecs
[ 2.798536] Doing 41
[ 2.798562] calling init_user_reserve+0x0/0xac @ 1
[ 2.798596] initcall init_user_reserve+0x0/0xac returned 0 after 1 usecs
[ 2.798613] Doing 42
[ 2.798643] calling proc_vmalloc_init+0x0/0x68 @ 1
[ 2.798693] initcall proc_vmalloc_init+0x0/0x68 returned 0 after 15 usecs
[ 2.798712] Doing 43
[ 2.798743] calling memblock_init_debugfs+0x0/0x98 @ 1
[ 2.798845] initcall memblock_init_debugfs+0x0/0x98 returned 0 after 63 usecs
[ 2.798864] Doing 44
[ 2.798895] calling init_emergency_pool+0x0/0xbc @ 1
[ 2.798930] initcall init_emergency_pool+0x0/0xbc returned 0 after 2 usecs
[ 2.798950] Doing 45
[ 2.798980] calling procswaps_init+0x0/0x68 @ 1
[ 2.799029] initcall procswaps_init+0x0/0x68 returned 0 after 15 usecs
[ 2.799049] Doing 46
[ 2.799076] calling ksm_init+0x0/0x11c @ 1
[ 2.799455] initcall ksm_init+0x0/0x11c returned 0 after 327 usecs
[ 2.799476] Doing 47
[ 2.799510] calling slab_sysfs_init+0x0/0x1c4 @ 1
[ 2.809432] initcall slab_sysfs_init+0x0/0x1c4 returned 0 after 9642 usecs
[ 2.809456] Doing 48
[ 2.809488] calling fcntl_init+0x0/0x50 @ 1
[ 2.809549] initcall fcntl_init+0x0/0x50 returned 0 after 25 usecs
[ 2.809570] Doing 49
[ 2.809597] calling proc_filesystems_init+0x0/0x68 @ 1
[ 2.809652] initcall proc_filesystems_init+0x0/0x68 returned 0 after 21 usecs
[ 2.809673] Doing 50
[ 2.809701] calling dio_init+0x0/0x50 @ 1
[ 2.809997] initcall dio_init+0x0/0x50 returned 0 after 258 usecs
[ 2.810017] Doing 51
[ 2.810045] calling fsnotify_mark_init+0x0/0x9c @ 1
[ 2.810330] initcall fsnotify_mark_init+0x0/0x9c returned 0 after 242 usecs
[ 2.810353] Doing 52
[ 2.810378] calling dnotify_init+0x0/0xd0 @ 1
[ 2.810753] initcall dnotify_init+0x0/0xd0 returned 0 after 330 usecs
[ 2.810774] Doing 53
[ 2.810804] calling inotify_user_setup+0x0/0xb0 @ 1
[ 2.810874] initcall inotify_user_setup+0x0/0xb0 returned 0 after 39 usecs
[ 2.810896] Doing 54
[ 2.810920] calling aio_setup+0x0/0x8c @ 1
[ 2.810993] initcall aio_setup+0x0/0x8c returned 0 after 41 usecs
[ 2.811012] Doing 55
[ 2.811040] calling proc_locks_init+0x0/0x68 @ 1
[ 2.811091] initcall proc_locks_init+0x0/0x68 returned 0 after 20 usecs
[ 2.811110] Doing 56
[ 2.811136] calling init_mbcache+0x0/0x24 @ 1
[ 2.811172] initcall init_mbcache+0x0/0x24 returned 0 after 5 usecs
[ 2.811189] Doing 57
[ 2.811214] calling dquot_init+0x0/0x248 @ 1
[ 2.811234] VFS: Disk quotas dquot_6.5.2
[ 2.812017] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 2.812056] initcall dquot_init+0x0/0x248 returned 0 after 791 usecs
[ 2.812075] Doing 58
[ 2.812100] calling quota_init+0x0/0x58 @ 1
[ 2.812174] initcall quota_init+0x0/0x58 returned 0 after 41 usecs
[ 2.812195] Doing 59
[ 2.812221] calling proc_cmdline_init+0x0/0x68 @ 1
[ 2.812271] initcall proc_cmdline_init+0x0/0x68 returned 0 after 17 usecs
[ 2.812290] Doing 60
[ 2.812317] calling proc_consoles_init+0x0/0x68 @ 1
[ 2.812361] initcall proc_consoles_init+0x0/0x68 returned 0 after 14 usecs
[ 2.812381] Doing 61
[ 2.812408] calling proc_cpuinfo_init+0x0/0x68 @ 1
[ 2.812452] initcall proc_cpuinfo_init+0x0/0x68 returned 0 after 14 usecs
[ 2.812471] Doing 62
[ 2.812497] calling proc_devices_init+0x0/0x68 @ 1
[ 2.812542] initcall proc_devices_init+0x0/0x68 returned 0 after 13 usecs
[ 2.812562] Doing 63
[ 2.812588] calling proc_interrupts_init+0x0/0x68 @ 1
[ 2.812632] initcall proc_interrupts_init+0x0/0x68 returned 0 after 13 usecs
[ 2.812651] Doing 64
[ 2.812678] calling proc_loadavg_init+0x0/0x68 @ 1
[ 2.812723] initcall proc_loadavg_init+0x0/0x68 returned 0 after 14 usecs
[ 2.812744] Doing 65
[ 2.812769] calling proc_meminfo_init+0x0/0x68 @ 1
[ 2.812816] initcall proc_meminfo_init+0x0/0x68 returned 0 after 14 usecs
[ 2.812836] Doing 66
[ 2.812864] calling proc_stat_init+0x0/0x68 @ 1
[ 2.812943] initcall proc_stat_init+0x0/0x68 returned 0 after 45 usecs
[ 2.812963] Doing 67
[ 2.812991] calling proc_uptime_init+0x0/0x68 @ 1
[ 2.813038] initcall proc_uptime_init+0x0/0x68 returned 0 after 14 usecs
[ 2.813058] Doing 68
[ 2.813086] calling proc_version_init+0x0/0x68 @ 1
[ 2.813133] initcall proc_version_init+0x0/0x68 returned 0 after 14 usecs
[ 2.813151] Doing 69
[ 2.813179] calling proc_softirqs_init+0x0/0x68 @ 1
[ 2.813224] initcall proc_softirqs_init+0x0/0x68 returned 0 after 14 usecs
[ 2.813243] Doing 70
[ 2.813270] calling proc_kmsg_init+0x0/0x68 @ 1
[ 2.813317] initcall proc_kmsg_init+0x0/0x68 returned 0 after 14 usecs
[ 2.813336] Doing 71
[ 2.813361] calling proc_page_init+0x0/0xb0 @ 1
[ 2.813419] initcall proc_page_init+0x0/0xb0 returned 0 after 27 usecs
[ 2.813438] Doing 72
[ 2.813463] calling configfs_init+0x0/0x148 @ 1
[ 2.814148] initcall configfs_init+0x0/0x148 returned 0 after 632 usecs
[ 2.814170] Doing 73
[ 2.814199] calling init_devpts_fs+0x0/0xc0 @ 1
[ 2.814753] initcall init_devpts_fs+0x0/0xc0 returned 0 after 504 usecs
[ 2.814776] Doing 74
[ 2.814807] calling init_ext3_fs+0x0/0x88 @ 1
[ 2.815359] initcall init_ext3_fs+0x0/0x88 returned 0 after 504 usecs
[ 2.815381] Doing 75
[ 2.815410] calling init_ext2_fs+0x0/0x88 @ 1
[ 2.815691] initcall init_ext2_fs+0x0/0x88 returned 0 after 243 usecs
[ 2.815714] Doing 76
[ 2.815748] calling ext4_init_fs+0x0/0x298 @ 1
[ 2.817225] initcall ext4_init_fs+0x0/0x298 returned 0 after 1402 usecs
[ 2.817248] Doing 77
[ 2.817281] calling journal_init+0x0/0x38 @ 1
[ 2.817873] initcall journal_init+0x0/0x38 returned 0 after 540 usecs
[ 2.817897] Doing 78
[ 2.817927] calling journal_init+0x0/0x40 @ 1
[ 2.818087] initcall journal_init+0x0/0x40 returned 0 after 121 usecs
[ 2.818107] Doing 79
[ 2.818137] calling init_ramfs_fs+0x0/0x24 @ 1
[ 2.818178] initcall init_ramfs_fs+0x0/0x24 returned 0 after 8 usecs
[ 2.818196] Doing 80
[ 2.818223] calling init_fat_fs+0x0/0x60 @ 1
[ 2.818723] initcall init_fat_fs+0x0/0x60 returned 0 after 452 usecs
[ 2.818745] Doing 81
[ 2.818774] calling init_vfat_fs+0x0/0x24 @ 1
[ 2.818814] initcall init_vfat_fs+0x0/0x24 returned 0 after 8 usecs
[ 2.818833] Doing 82
[ 2.818861] calling init_msdos_fs+0x0/0x24 @ 1
[ 2.818901] initcall init_msdos_fs+0x0/0x24 returned 0 after 7 usecs
[ 2.818919] Doing 83
[ 2.818949] calling init_iso9660_fs+0x0/0x88 @ 1
[ 2.819495] initcall init_iso9660_fs+0x0/0x88 returned 0 after 487 usecs
[ 2.819516] Doing 84
[ 2.819547] calling init_nfs_fs+0x0/0x1b0 @ 1
[ 2.821193] initcall init_nfs_fs+0x0/0x1b0 returned 0 after 1562 usecs
[ 2.821219] Doing 85
[ 2.821249] calling init_nfs_v2+0x0/0x24 @ 1
[ 2.821285] initcall init_nfs_v2+0x0/0x24 returned 0 after 2 usecs
[ 2.821304] Doing 86
[ 2.821332] calling init_nfs_v3+0x0/0x24 @ 1
[ 2.821365] initcall init_nfs_v3+0x0/0x24 returned 0 after 2 usecs
[ 2.821384] Doing 87
[ 2.821411] calling init_nfs_v4+0x0/0x6c @ 1
[ 2.821432] NFS: Registering the id_resolver key type
[ 2.821530] Key type id_resolver registered
[ 2.821558] Key type id_legacy registered
[ 2.821624] initcall init_nfs_v4+0x0/0x6c returned 0 after 172 usecs
[ 2.821645] Doing 88
[ 2.821674] calling init_nlm+0x0/0x9c @ 1
[ 2.821756] initcall init_nlm+0x0/0x9c returned 0 after 46 usecs
[ 2.821777] Doing 89
[ 2.821808] calling init_nls_cp437+0x0/0x24 @ 1
[ 2.821842] initcall init_nls_cp437+0x0/0x24 returned 0 after 2 usecs
[ 2.821861] Doing 90
[ 2.821890] calling init_nls_ascii+0x0/0x24 @ 1
[ 2.821925] initcall init_nls_ascii+0x0/0x24 returned 0 after 2 usecs
[ 2.821943] Doing 91
[ 2.821972] calling init_nls_iso8859_1+0x0/0x24 @ 1
[ 2.822007] initcall init_nls_iso8859_1+0x0/0x24 returned 0 after 2 usecs
[ 2.822025] Doing 92
[ 2.822054] calling init_nls_iso8859_15+0x0/0x24 @ 1
[ 2.822089] initcall init_nls_iso8859_15+0x0/0x24 returned 0 after 2 usecs
[ 2.822108] Doing 93
[ 2.822138] calling init_nls_utf8+0x0/0x6c @ 1
[ 2.822175] initcall init_nls_utf8+0x0/0x6c returned 0 after 6 usecs
[ 2.822193] Doing 94
[ 2.822220] calling init_ntfs_fs+0x0/0x32c @ 1
[ 2.822239] NTFS driver 2.1.30 [Flags: R/W DEBUG].
[ 2.822899] initcall init_ntfs_fs+0x0/0x32c returned 0 after 623 usecs
[ 2.822922] Doing 95
[ 2.822953] calling init_jffs2_fs+0x0/0x124 @ 1
[ 2.822974] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 2.825337] initcall init_jffs2_fs+0x0/0x124 returned 0 after 2279 usecs
[ 2.825365] Doing 96
[ 2.825397] calling init_autofs4_fs+0x0/0x44 @ 1
[ 2.825840] initcall init_autofs4_fs+0x0/0x44 returned 0 after 392 usecs
[ 2.825864] Doing 97
[ 2.825895] calling fuse_init+0x0/0xf0 @ 1
[ 2.825918] fuse init (API version 7.22)
[ 2.826833] initcall fuse_init+0x0/0xf0 returned 0 after 875 usecs
[ 2.826858] Doing 98
[ 2.826887] calling init_udf_fs+0x0/0x68 @ 1
[ 2.827199] initcall init_udf_fs+0x0/0x68 returned 0 after 274 usecs
[ 2.827221] Doing 99
[ 2.827247] calling init_pstore_fs+0x0/0xa4 @ 1
[ 2.827306] initcall init_pstore_fs+0x0/0xa4 returned 0 after 27 usecs
[ 2.827326] Doing 100
[ 2.827351] calling ipc_init+0x0/0x30 @ 1
[ 2.827406] msgmni has been set to 1965
[ 2.827468] initcall ipc_init+0x0/0x30 returned 0 after 84 usecs
[ 2.827487] Doing 101
[ 2.827515] calling ipc_sysctl_init+0x0/0x24 @ 1
[ 2.827607] initcall ipc_sysctl_init+0x0/0x24 returned 0 after 58 usecs
[ 2.827627] Doing 102
[ 2.827654] calling key_proc_init+0x0/0x88 @ 1
[ 2.827703] initcall key_proc_init+0x0/0x88 returned 0 after 19 usecs
[ 2.827726] Doing 103
[ 2.827753] calling selinux_nf_ip_init+0x0/0xac @ 1
[ 2.827773] SELinux: Registering netfilter hooks
[ 2.827806] initcall selinux_nf_ip_init+0x0/0xac returned 0 after 24 usecs
[ 2.827823] Doing 104
[ 2.827848] calling init_sel_fs+0x0/0x150 @ 1
[ 2.829091] initcall init_sel_fs+0x0/0x150 returned 0 after 1179 usecs
[ 2.829113] Doing 105
[ 2.829140] calling selnl_init+0x0/0xd4 @ 1
[ 2.829202] initcall selnl_init+0x0/0xd4 returned 0 after 29 usecs
[ 2.829224] Doing 106
[ 2.829251] calling sel_netif_init+0x0/0xcc @ 1
[ 2.829295] initcall sel_netif_init+0x0/0xcc returned 0 after 12 usecs
[ 2.829314] Doing 107
[ 2.829341] calling sel_netnode_init+0x0/0xf8 @ 1
[ 2.829383] initcall sel_netnode_init+0x0/0xf8 returned 0 after 13 usecs
[ 2.829402] Doing 108
[ 2.829428] calling sel_netport_init+0x0/0xf8 @ 1
[ 2.829471] initcall sel_netport_init+0x0/0xf8 returned 0 after 14 usecs
[ 2.829490] Doing 109
[ 2.829516] calling aurule_init+0x0/0x50 @ 1
[ 2.829546] initcall aurule_init+0x0/0x50 returned 0 after 3 usecs
[ 2.829565] Doing 110
[ 2.829590] calling crypto_algapi_init+0x0/0x1c @ 1
[ 2.829647] initcall crypto_algapi_init+0x0/0x1c returned 0 after 24 usecs
[ 2.829666] Doing 111
[ 2.829692] calling skcipher_module_init+0x0/0x78 @ 1
[ 2.829724] initcall skcipher_module_init+0x0/0x78 returned 0 after 1 usecs
[ 2.829742] Doing 112
[ 2.829768] calling chainiv_module_init+0x0/0x24 @ 1
[ 2.829803] initcall chainiv_module_init+0x0/0x24 returned 0 after 6 usecs
[ 2.829822] Doing 113
[ 2.829847] calling eseqiv_module_init+0x0/0x24 @ 1
[ 2.829879] initcall eseqiv_module_init+0x0/0x24 returned 0 after 3 usecs
[ 2.829898] Doing 114
[ 2.829923] calling seqiv_module_init+0x0/0x24 @ 1
[ 2.829958] initcall seqiv_module_init+0x0/0x24 returned 0 after 4 usecs
[ 2.829975] Doing 115
[ 2.830004] calling crypto_user_init+0x0/0xcc @ 1
[ 2.830055] initcall crypto_user_init+0x0/0xcc returned 0 after 20 usecs
[ 2.830079] Doing 116
[ 2.830106] calling hmac_module_init+0x0/0x24 @ 1
[ 2.830139] initcall hmac_module_init+0x0/0x24 returned 0 after 4 usecs
[ 2.830160] Doing 117
[ 2.830188] calling crypto_null_mod_init+0x0/0x88 @ 1
[ 2.831507] initcall crypto_null_mod_init+0x0/0x88 returned 0 after 1247 usecs
[ 2.831534] Doing 118
[ 2.831563] calling md4_mod_init+0x0/0x24 @ 1
[ 2.831849] initcall md4_mod_init+0x0/0x24 returned 0 after 244 usecs
[ 2.831872] Doing 119
[ 2.831900] calling md5_mod_init+0x0/0x24 @ 1
[ 2.832184] initcall md5_mod_init+0x0/0x24 returned 0 after 242 usecs
[ 2.832207] Doing 120
[ 2.832234] calling rmd128_mod_init+0x0/0x24 @ 1
[ 2.832513] initcall rmd128_mod_init+0x0/0x24 returned 0 after 237 usecs
[ 2.832537] Doing 121
[ 2.832564] calling rmd160_mod_init+0x0/0x24 @ 1
[ 2.832846] initcall rmd160_mod_init+0x0/0x24 returned 0 after 240 usecs
[ 2.832869] Doing 122
[ 2.832898] calling rmd256_mod_init+0x0/0x24 @ 1
[ 2.833176] initcall rmd256_mod_init+0x0/0x24 returned 0 after 238 usecs
[ 2.833199] Doing 123
[ 2.833226] calling rmd320_mod_init+0x0/0x24 @ 1
[ 2.833503] initcall rmd320_mod_init+0x0/0x24 returned 0 after 234 usecs
[ 2.833527] Doing 124
[ 2.833554] calling sha1_generic_mod_init+0x0/0x24 @ 1
[ 2.833833] initcall sha1_generic_mod_init+0x0/0x24 returned 0 after 236 usecs
[ 2.833860] Doing 125
[ 2.833891] calling sha256_generic_mod_init+0x0/0x28 @ 1
[ 2.834564] initcall sha256_generic_mod_init+0x0/0x28 returned 0 after 618 usecs
[ 2.834590] Doing 126
[ 2.834622] calling sha512_generic_mod_init+0x0/0x28 @ 1
[ 2.835184] initcall sha512_generic_mod_init+0x0/0x28 returned 0 after 512 usecs
[ 2.835208] Doing 127
[ 2.835235] calling wp512_mod_init+0x0/0x28 @ 1
[ 2.836049] initcall wp512_mod_init+0x0/0x28 returned 0 after 758 usecs
[ 2.836073] Doing 128
[ 2.836101] calling tgr192_mod_init+0x0/0x28 @ 1
[ 2.836869] initcall tgr192_mod_init+0x0/0x28 returned 0 after 712 usecs
[ 2.836894] Doing 129
[ 2.836924] calling crypto_ecb_module_init+0x0/0x24 @ 1
[ 2.836962] initcall crypto_ecb_module_init+0x0/0x24 returned 0 after 5 usecs
[ 2.836981] Doing 130
[ 2.837008] calling crypto_cbc_module_init+0x0/0x24 @ 1
[ 2.837041] initcall crypto_cbc_module_init+0x0/0x24 returned 0 after 3 usecs
[ 2.837061] Doing 131
[ 2.837088] calling crypto_cts_module_init+0x0/0x24 @ 1
[ 2.837122] initcall crypto_cts_module_init+0x0/0x24 returned 0 after 4 usecs
[ 2.837141] Doing 132
[ 2.837166] calling crypto_module_init+0x0/0x24 @ 1
[ 2.837198] initcall crypto_module_init+0x0/0x24 returned 0 after 3 usecs
[ 2.837219] Doing 133
[ 2.837245] calling crypto_module_init+0x0/0x24 @ 1
[ 2.837278] initcall crypto_module_init+0x0/0x24 returned 0 after 4 usecs
[ 2.837296] Doing 134
[ 2.837321] calling crypto_ctr_module_init+0x0/0x74 @ 1
[ 2.837358] initcall crypto_ctr_module_init+0x0/0x74 returned 0 after 7 usecs
[ 2.837376] Doing 135
[ 2.837402] calling crypto_gcm_module_init+0x0/0x14c @ 1
[ 2.837451] initcall crypto_gcm_module_init+0x0/0x14c returned 0 after 18 usecs
[ 2.837470] Doing 136
[ 2.837496] calling crypto_ccm_module_init+0x0/0xa4 @ 1
[ 2.837537] initcall crypto_ccm_module_init+0x0/0xa4 returned 0 after 11 usecs
[ 2.837556] Doing 137
[ 2.837583] calling des_generic_mod_init+0x0/0x28 @ 1
[ 2.838115] initcall des_generic_mod_init+0x0/0x28 returned 0 after 483 usecs
[ 2.838140] Doing 138
[ 2.838169] calling blowfish_mod_init+0x0/0x24 @ 1
[ 2.838530] initcall blowfish_mod_init+0x0/0x24 returned 0 after 317 usecs
[ 2.838555] Doing 139
[ 2.838584] calling twofish_mod_init+0x0/0x24 @ 1
[ 2.838875] initcall twofish_mod_init+0x0/0x24 returned 0 after 244 usecs
[ 2.838899] Doing 140
[ 2.838926] calling aes_init+0x0/0x24 @ 1
[ 2.839207] initcall aes_init+0x0/0x24 returned 0 after 239 usecs
[ 2.839230] Doing 141
[ 2.839259] calling camellia_init+0x0/0x24 @ 1
[ 2.839548] initcall camellia_init+0x0/0x24 returned 0 after 246 usecs
[ 2.839571] Doing 142
[ 2.839599] calling arc4_init+0x0/0x28 @ 1
[ 2.840128] initcall arc4_init+0x0/0x28 returned 0 after 480 usecs
[ 2.840152] Doing 143
[ 2.840180] calling deflate_mod_init+0x0/0x24 @ 1
[ 2.840463] initcall deflate_mod_init+0x0/0x24 returned 0 after 239 usecs
[ 2.840488] Doing 144
[ 2.840517] calling michael_mic_init+0x0/0x24 @ 1
[ 2.840804] initcall michael_mic_init+0x0/0x24 returned 0 after 244 usecs
[ 2.840828] Doing 145
[ 2.840856] calling crc32c_mod_init+0x0/0x24 @ 1
[ 2.841196] initcall crc32c_mod_init+0x0/0x24 returned 0 after 295 usecs
[ 2.841219] Doing 146
[ 2.841251] calling crypto_authenc_module_init+0x0/0x24 @ 1
[ 2.841291] initcall crypto_authenc_module_init+0x0/0x24 returned 0 after 8 usecs
[ 2.841311] Doing 147
[ 2.841338] calling crypto_authenc_esn_module_init+0x0/0x24 @ 1
[ 2.841372] initcall crypto_authenc_esn_module_init+0x0/0x24 returned 0 after 3 usecs
[ 2.841391] Doing 148
[ 2.841416] calling lzo_mod_init+0x0/0x24 @ 1
[ 2.841698] initcall lzo_mod_init+0x0/0x24 returned 0 after 240 usecs
[ 2.841723] Doing 149
[ 2.841751] calling krng_mod_init+0x0/0x24 @ 1
[ 2.842071] initcall krng_mod_init+0x0/0x24 returned 0 after 276 usecs
[ 2.842094] Doing 150
[ 2.842123] calling ghash_mod_init+0x0/0x24 @ 1
[ 2.842419] initcall ghash_mod_init+0x0/0x24 returned 0 after 250 usecs
[ 2.842442] Doing 151
[ 2.842473] calling proc_genhd_init+0x0/0xb0 @ 1
[ 2.842551] initcall proc_genhd_init+0x0/0xb0 returned 0 after 43 usecs
[ 2.842573] Doing 152
[ 2.842602] calling noop_init+0x0/0x24 @ 1
[ 2.842625] io scheduler noop registered
[ 2.842654] initcall noop_init+0x0/0x24 returned 0 after 22 usecs
[ 2.842672] Doing 153
[ 2.842699] calling deadline_init+0x0/0x24 @ 1
[ 2.842721] io scheduler deadline registered
[ 2.842752] initcall deadline_init+0x0/0x24 returned 0 after 23 usecs
[ 2.842773] Doing 154
[ 2.842798] calling cfq_init+0x0/0x108 @ 1
[ 2.843228] io scheduler cfq registered (default)
[ 2.843266] initcall cfq_init+0x0/0x108 returned 0 after 423 usecs
[ 2.843286] Doing 155
[ 2.843317] calling libcrc32c_mod_init+0x0/0x84 @ 1
[ 2.843371] initcall libcrc32c_mod_init+0x0/0x84 returned 0 after 21 usecs
[ 2.843390] Doing 156
[ 2.843416] calling init_kmp+0x0/0x24 @ 1
[ 2.843448] initcall init_kmp+0x0/0x24 returned 0 after 2 usecs
[ 2.843466] Doing 157
[ 2.843492] calling init_bm+0x0/0x24 @ 1
[ 2.843523] initcall init_bm+0x0/0x24 returned 0 after 2 usecs
[ 2.843541] Doing 158
[ 2.843567] calling init_fsm+0x0/0x24 @ 1
[ 2.843597] initcall init_fsm+0x0/0x24 returned 0 after 2 usecs
[ 2.843616] Doing 159
[ 2.843644] calling percpu_counter_startup+0x0/0x28 @ 1
[ 2.843682] initcall percpu_counter_startup+0x0/0x28 returned 0 after 7 usecs
[ 2.843702] Doing 160
[ 2.843729] calling audit_classes_init+0x0/0x68 @ 1
[ 2.843775] initcall audit_classes_init+0x0/0x68 returned 0 after 13 usecs
[ 2.843795] Doing 161
[ 2.843825] calling weim_driver_init+0x0/0x24 @ 1
[ 2.844472] imx-weim 21b8000.weim: WEIM driver registered.
[ 2.844769] initcall weim_driver_init+0x0/0x24 returned 0 after 883 usecs
[ 2.844792] Doing 162
[ 2.844825] calling imx_pwm_driver_init+0x0/0x24 @ 1
[ 2.846388] initcall imx_pwm_driver_init+0x0/0x24 returned 0 after 1484 usecs
[ 2.846411] Doing 163
[ 2.846443] calling pci_proc_init+0x0/0xd4 @ 1
[ 2.846551] initcall pci_proc_init+0x0/0xd4 returned 0 after 68 usecs
[ 2.846571] Doing 164
[ 2.846602] calling pcie_portdrv_init+0x0/0xb4 @ 1
[ 2.847531] initcall pcie_portdrv_init+0x0/0xb4 returned 0 after 868 usecs
[ 2.847555] Doing 165
[ 2.847587] calling aer_service_init+0x0/0x50 @ 1
[ 2.847854] aer 0000:00:00.0:pcie02: service driver aer loaded
[ 2.847948] initcall aer_service_init+0x0/0x50 returned 0 after 318 usecs
[ 2.847969] Doing 166
[ 2.848002] calling pcie_pme_service_init+0x0/0x24 @ 1
[ 2.848171] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 2.848212] pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded
[ 2.848306] initcall pcie_pme_service_init+0x0/0x24 returned 0 after 258 usecs
[ 2.848328] Doing 167
[ 2.848358] calling fb_console_init+0x0/0x114 @ 1
[ 2.848559] initcall fb_console_init+0x0/0x114 returned 0 after 162 usecs
[ 2.848581] Doing 168
[ 2.848615] calling l4f00242t03_driver_init+0x0/0x24 @ 1
[ 2.848714] initcall l4f00242t03_driver_init+0x0/0x24 returned 0 after 63 usecs
[ 2.848735] Doing 169
[ 2.848765] calling platform_lcd_driver_init+0x0/0x24 @ 1
[ 2.849304] initcall platform_lcd_driver_init+0x0/0x24 returned 0 after 487 usecs
[ 2.849327] Doing 170
[ 2.849358] calling genericbl_driver_init+0x0/0x24 @ 1
[ 2.849610] initcall genericbl_driver_init+0x0/0x24 returned 0 after 208 usecs
[ 2.849632] Doing 171
[ 2.849662] calling pwm_backlight_driver_init+0x0/0x24 @ 1
[ 2.851550] imx-pwm 2084000.pwm: pwm enabled
[ 2.904465] initcall pwm_backlight_driver_init+0x0/0x24 returned 0 after 53472 usecs
[ 2.904492] Doing 172
[ 2.904521] calling ldb_driver_init+0x0/0x24 @ 1
[ 2.906488] initcall ldb_driver_init+0x0/0x24 returned 0 after 1879 usecs
[ 2.906511] Doing 173
[ 2.906543] calling mipi_dsi_init+0x0/0x5c @ 1
[ 2.907254] MIPI DSI driver module loaded
[ 2.907293] initcall mipi_dsi_init+0x0/0x5c returned 0 after 697 usecs
[ 2.907313] Doing 174
[ 2.907343] calling mxc_hdmi_i2c_init+0x0/0x28 @ 1
[ 2.907615] initcall mxc_hdmi_i2c_init+0x0/0x28 returned 0 after 226 usecs
[ 2.907638] Doing 175
[ 2.907667] calling mxc_hdmi_init+0x0/0x24 @ 1
[ 2.909310] initcall mxc_hdmi_init+0x0/0x24 returned 0 after 1562 usecs
[ 2.909336] Doing 176
[ 2.909365] calling mxc_lcdif_init+0x0/0x24 @ 1
[ 2.909895] initcall mxc_lcdif_init+0x0/0x24 returned 0 after 480 usecs
[ 2.909918] Doing 177
[ 2.909949] calling mxcfb_init+0x0/0x24 @ 1
[ 2.910597] mxc_sdc_fb fb.24: registered mxc display driver ldb
[ 2.954454] imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 3.172492] Console: switching to colour frame buffer device 128x37
[ 3.210270] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[ 3.210326] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[ 3.210515] mxc_sdc_fb fb.25: registered mxc display driver hdmi
[ 3.320320] mxc_sdc_fb fb.26: Can't get fb option for mxcfb2!
[ 3.320521] mxc_sdc_fb fb.27: Can't get fb option for mxcfb3!
[ 3.320699] initcall mxcfb_init+0x0/0x24 returned 0 after 401079 usecs
[ 3.320722] Doing 178
[ 3.320755] calling mxc_epdc_fb_driver_init+0x0/0x24 @ 1
[ 3.321365] initcall mxc_epdc_fb_driver_init+0x0/0x24 returned 0 after 558 usecs
[ 3.321388] Doing 179
[ 3.321419] calling sii902x_driver_init+0x0/0x28 @ 1
[ 3.321589] initcall sii902x_driver_init+0x0/0x28 returned 0 after 131 usecs
[ 3.321611] Doing 180
[ 3.321641] calling cabc_driver_init+0x0/0x24 @ 1
[ 3.322098] initcall cabc_driver_init+0x0/0x24 returned 0 after 411 usecs
[ 3.322118] Doing 181
[ 3.322148] calling mx3fb_init+0x0/0x4c @ 1
[ 3.322398] initcall mx3fb_init+0x0/0x4c returned 0 after 210 usecs
[ 3.322418] Doing 182
[ 3.322446] calling mxsfb_driver_init+0x0/0x24 @ 1
[ 3.323124] initcall mxsfb_driver_init+0x0/0x24 returned 0 after 627 usecs
[ 3.323144] Doing 183
[ 3.323174] calling pxp_driver_init+0x0/0x24 @ 1
[ 3.323665] initcall pxp_driver_init+0x0/0x24 returned 0 after 445 usecs
[ 3.323687] Doing 184
[ 3.323716] calling sdma_module_init+0x0/0x2c @ 1
[ 3.324406] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 3.329132] imx-sdma 20ec000.sdma: loaded firmware 1.1
[ 3.336107] imx-sdma 20ec000.sdma: initialized
[ 3.336612] initcall sdma_module_init+0x0/0x2c returned 0 after 12549 usecs
[ 3.336634] Doing 185
[ 3.336667] calling pfuze_driver_init+0x0/0x28 @ 1
[ 3.338582] pfuze100-regulator 1-0008: Full lay: 2, Metal lay: 1
[ 3.339328] pfuze100-regulator 1-0008: FAB: 0, FIN: 0
[ 3.339361] pfuze100-regulator 1-0008: pfuze100 found.
[ 3.341469] SW1AB: 300 <--> 1875 mV at 1150 mV
[ 3.343964] SW1C: 300 <--> 1875 mV at 1175 mV
[ 3.346466] SW2: 800 <--> 3300 mV at 3300 mV
[ 3.348991] SW3A: 400 <--> 1975 mV at 1350 mV
[ 3.351468] SW3B: 400 <--> 1975 mV at 1350 mV
[ 3.354056] SW4: 800 <--> 1975 mV at 1800 mV
[ 3.355891] SWBST: 5000 <--> 5150 mV at 5000 mV
[ 3.357639] VSNVS: 1000 <--> 3000 mV at 3000 mV
[ 3.358704] VREFDDR: 750 mV
[ 3.359735] VGEN1: 800 <--> 1550 mV at 1200 mV
[ 3.361530] VGEN2: 800 <--> 1550 mV at 1500 mV
[ 3.364167] VGEN3: 1800 <--> 3300 mV at 2800 mV
[ 3.366740] VGEN4: 1800 <--> 3300 mV at 3300 mV
[ 3.369245] VGEN5: 1800 <--> 3300 mV at 3300 mV
[ 3.371714] VGEN6: 1800 <--> 3300 mV at 3000 mV
[ 3.375737] VCOIN: 3000 mV
[ 3.376800] initcall pfuze_driver_init+0x0/0x28 returned 0 after | usecs
[ 3.376825] Doing 186 |
[ 3.376858] calling pty_init+0x0/0x1c @ 1
[ 3.377261] initcall pty_init+0x0/0x1c returned 0 after 355 usecs
[ 3.377286] Doing 187
[ 3.377317] calling sysrq_init+0x0/0x104 @ 1
[ 3.377392] initcall sysrq_init+0x0/0x104 returned 0 after 40 usecs
[ 3.377411] Doing 188
[ 3.377441] calling imx_serial_init+0x0/0x78 @ 1
[ 3.377459] Serial: IMX driver
[ 3.378182] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
[ 9.706144] console [ttymxc0] enabled
[ 9.711306] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
[ 9.719339] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
[ 9.727160] 21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
[ 9.734940] initcall imx_serial_init+0x0/0x78 returned 0 after 6208452 usecs
[ 9.742022] Doing 189
[ 9.744384] calling init_kgdboc+0x0/0x38 @ 1
[ 9.748800] kgdb: Registered I/O driver kgdboc.
[ 9.753371] kgdb: Waiting for connection from remote gdb...