I.mx6 parallel lcd DISP0_CLK level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mx6 parallel lcd DISP0_CLK level

1,233 Views
gtkim
Contributor I

Dear ALL

I test & checking in sabreSD board parallel LCD interface.

But i find starange porint in parallel lcd interface hw signal level by osilloscope..

Allmost signal is operation in 0V~3.3V.

But only DISP0_CLK is diffienct other signal, it's operation in 1V~2.2V.

Now no connection state parallel lcd module.

I checking complete change frequency as specify value.

Plz help & reply, is it normal state?

Thanks..

0 Kudos
Reply
0 Replies