WMA/WMV decode by i.MX6S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WMA/WMV decode by i.MX6S

Jump to solution
2,198 Views
kanoumamoru
Contributor III

I want to decode WMA/WMV file to try to check for windows media files.

Where can I find the WMV/WMA codec support ?

I can't find out these in the LTIB package when building with MMCODEC.

If it needs license agreement, do we have to contact microsoft ?

Best Regards,

kanou

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
1,582 Views
Yuri
NXP Employee
NXP Employee

Please apply to local Freescale FAE.

Windows Media Components Final Product Licensee should be approved prior to distribution.

View solution in original post

0 Kudos
Reply
2 Replies
1,583 Views
Yuri
NXP Employee
NXP Employee

Please apply to local Freescale FAE.

Windows Media Components Final Product Licensee should be approved prior to distribution.

0 Kudos
Reply
1,582 Views
srinivasanshanm
Contributor III

Dear I.MX Community,

I am using L2.6.35_1.1.0_130130_source for my I.MX28 customized platform,

I am trying to play .wma songs using gplay, but the .wma songs which has album art is not playing, & .wma songs which has metadata is also not getting played,

As am new to this .wma software codec, could  you please let me know how to resolve this issue, & necessary configurations that is to be done

in the ltib, inorder to get the the wma songs with album art & metadata getting played

Could you please let me know the detailed ltib configurations that needs to be done in order to get the wma songs to be played with album art & metadata

WMA with album art not working LOGs

gplay test.wma

playbin2 is employed!

fsl_player_init(): Successfully initialize!

fsl_player_set_media_location(): filename=/03 - Mahiya - Suzzane.wma

[Stopped  ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.6

Core: ASFPARSER_01.00.14  build on Dec 10 2012 15:58:36

  mime: video/x-ms-asf

  file: /usr/lib/imx-mm/parser/lib_asf_parser_arm9_elinux.so.3.1

Content Info:

        URI:

              file:///03 - Mahiya - Suzzane.wma

        Idx File:

              /root/.aiur/.03 - Mahiya - Suzzane.wma.aidx

        Seekable  : Yes

        Size(byte): 1657511

[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4

[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4

[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4

[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4

Please kindly do the needful as early as possible, as am stuck with this from many days,

Many Advanced Thanks,

0 Kudos
Reply