I.mx6 PCIe clock setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.mx6 PCIe clock setting

1,977件の閲覧回数
karthikas
Contributor IV

Hello..,

I am using I.mx6 processor, In that I need to configure the PCIe

1.Please can anyone give me clear steps and which register I need to use to enable clock for PCIe.

2.PLL6 is used to generate clock for the PCIe.

ラベル(1)
タグ(2)
1 返信

1,524件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi KARTHIK

most full explanation of PCIe settings is provided on  i.MX6Q PCIe EP/RC Validation System

page :

https://community.freescale.com/docs/DOC-95014

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------