I.mx6 PCIe clock setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mx6 PCIe clock setting

1,976 Views
karthikas
Contributor IV

Hello..,

I am using I.mx6 processor, In that I need to configure the PCIe

1.Please can anyone give me clear steps and which register I need to use to enable clock for PCIe.

2.PLL6 is used to generate clock for the PCIe.

Labels (1)
Tags (2)
1 Reply

1,523 Views
igorpadykov
NXP Employee
NXP Employee

Hi KARTHIK

most full explanation of PCIe settings is provided on  i.MX6Q PCIe EP/RC Validation System

page :

https://community.freescale.com/docs/DOC-95014

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------