I.mx 8 Mini maximum RAM size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mx 8 Mini maximum RAM size?

Jump to solution
6,744 Views
ivo_kamalis
Contributor I

What is maximum RAM size SOC supports? I am planning to have 4 chips in 2 rank system? Is it 8 GB (4 pcs 16Gb 16bit modules)?

Tags (2)
1 Solution
6,518 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivo

for ddr memory support one can look at sect.2.1.1.3, 2.1.2 Cortex-A53 Memory Map,

sect.9.2.1.2 Features, sect.9.3.1.1 Features

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
6,519 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivo

for ddr memory support one can look at sect.2.1.1.3, 2.1.2 Cortex-A53 Memory Map,

sect.9.2.1.2 Features, sect.9.3.1.1 Features

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
6,518 Views
peterlischer
Senior Contributor I

Hi igorpadykov‌

As you replied Ivo half a year ago, the maximum addressable DDR memory size can be found in the reference manual. In section 2.1.2, I found this table: 

pastedImage_1.png

For the first 5GByte region, the description says "Quad-A53 only". Does this mean that the Dual, DualLite, Solo, and SoloLite can only address 3GByte? 

Any clarification would be very helpful. 

6,518 Views
malachi_burke
Contributor I

peterlischer‌ it sure seems that way

igorpadykov I'm also curious, since we're using i.MX 8M Mini also (Variscite's DART-MX8M-MINI) though it seems this vendor limits to 4GB currently

0 Kudos
Reply
6,518 Views
igorpadykov
NXP Employee
NXP Employee

Hi Malachi

max. size is described in sect.2.1.2 Cortex-A53 Memory Map as

replied above. Vendors may choose own configurations based on

specific design requirements.

Best regards
igor

0 Kudos
Reply
6,518 Views
malachi_burke
Contributor I

OK thank you.  I was getting confused I believe with manual IMX8MDQLQRM "i.MX 8M Dual/8M QuadLite/8M Quad" - looks like a red herring.

0 Kudos
Reply