I.mx 8 Mini maximum RAM size?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.mx 8 Mini maximum RAM size?

ソリューションへジャンプ
6,743件の閲覧回数
ivo_kamalis
Contributor I

What is maximum RAM size SOC supports? I am planning to have 4 chips in 2 rank system? Is it 8 GB (4 pcs 16Gb 16bit modules)?

タグ(2)
1 解決策
6,517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivo

for ddr memory support one can look at sect.2.1.1.3, 2.1.2 Cortex-A53 Memory Map,

sect.9.2.1.2 Features, sect.9.3.1.1 Features

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,518件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivo

for ddr memory support one can look at sect.2.1.1.3, 2.1.2 Cortex-A53 Memory Map,

sect.9.2.1.2 Features, sect.9.3.1.1 Features

i.MX 8M Mini Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
6,517件の閲覧回数
peterlischer
Senior Contributor I

Hi igorpadykov‌

As you replied Ivo half a year ago, the maximum addressable DDR memory size can be found in the reference manual. In section 2.1.2, I found this table: 

pastedImage_1.png

For the first 5GByte region, the description says "Quad-A53 only". Does this mean that the Dual, DualLite, Solo, and SoloLite can only address 3GByte? 

Any clarification would be very helpful. 

6,517件の閲覧回数
malachi_burke
Contributor I

peterlischer‌ it sure seems that way

igorpadykov I'm also curious, since we're using i.MX 8M Mini also (Variscite's DART-MX8M-MINI) though it seems this vendor limits to 4GB currently

0 件の賞賛
返信
6,517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Malachi

max. size is described in sect.2.1.2 Cortex-A53 Memory Map as

replied above. Vendors may choose own configurations based on

specific design requirements.

Best regards
igor

0 件の賞賛
返信
6,517件の閲覧回数
malachi_burke
Contributor I

OK thank you.  I was getting confused I believe with manual IMX8MDQLQRM "i.MX 8M Dual/8M QuadLite/8M Quad" - looks like a red herring.

0 件の賞賛
返信