I have received "Tx Message Buffer is currently in use".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have received "Tx Message Buffer is currently in use".

1,078 Views
Ayhan14
Contributor II

Hello,

When I used "CAN_Send" function in where is defined "CAN.c"  file, CAN messages is transmitted. However, When I wanted to use this function on "main.c" file I have received "Tx Message Buffer is currently in use". I included header files. Why do I can not transmit CAN messages on main function?

 

Regards,

Oğuzhan Ayhan

0 Kudos
Reply
2 Replies

1,030 Views
Ayhan14
Contributor II

Hello,

I had added but I did not send CAN messages due to same problem (Tx Message Buffer is currently in use)

Regards

0 Kudos
Reply

1,060 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Just add the header file where you want to take it.

Regards

0 Kudos
Reply