I do not use gpio to reset phy KSZ8041FTLI when use the clock generated by CPU(imx6q)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I do not use gpio to reset phy KSZ8041FTLI when use the clock generated by CPU(imx6q)

1,534 次查看
qumai
Contributor I

  I use the 50M clock generated by the CPU to provide the working clock for the PHY RMII interface,but I used a power-on reset to reset the PHY and CPU at the same time,not a GPIO reset.Thousands of boards which use the on chip clock generator, are currently produced, and the work is quite stable. but in the document IMX6DQ6SDLHDG,on the page 109,the schematic notes that PHY_ RESET_B must be a GPIO toggled after CLKIN is active.

  My question is How big the risk of network disconnection due to the wrong reset and clock sequence? My client wants to know How big is the risk .

   Now that the circuit board card reserves the position of the external 50M clock crystal oscillator for the phy, is it necessary to change to an external crystal oscillator to reduce the risk of network failure without redesigning the circuit board.

 Looking forward to your reply!

0 项奖励
回复
1 回复

1,531 次查看
igorpadykov
NXP Employee
NXP Employee

Hi qumai

 

this may depend on used transceiver chip, for KSZ8041 case recommended to

folow sect. 7.10 Reset Timing datasheet

KSZ8041TL/FTL/ML - 10Base-T/100Base-TX/100Base-FX PHY

 

Best regards
igor

0 项奖励
回复