Hello,
I work with imx7, I changed the linux kernel start address. I work with linux 4.9.11. I changed files:
- arch/arm/Kconfig I deleted line select AUTO_ZRELADDR in config ARCH_MULTIPLATFORM
- arch/arm/Makefile I added line MACHINE := arch/arm/mach-imx
- creat file arch/arm/march-imx/Makefile.boot with zreladdr-y += 0x81008000
params_phys-y := 0x81000100
initrd_phys-y := 0x81800000
If I build the linux-imx without clean it is ok. BUt if I clean I error with vmlinux.
/work_disk/fsl-arm-yocto-bsp/build_sabreimx7/tmp/work-shared/imx7dsabreca/kernel-source/Makefile:969: recipe for target 'vmlinux' failed
| make[2]: *** [vmlinux] Error 1
| Makefile:150: recipe for target 'sub-make' failed
| make[1]: *** [sub-make] Error 2
| Makefile:24: recipe for target '__sub-make' failed
| make: *** [__sub-make] Error 2
| WARNING: exit code 1 from a shell command.
Can you help me?
Best regard,
Francois.