I am not able build kernel-imx-gpu-viv in yocto project for imx7ulp board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am not able build kernel-imx-gpu-viv in yocto project for imx7ulp board

1,629件の閲覧回数
ravicalm
Contributor I

bitbake kernel-module-imx-gpu-viv
WARNING: You have included the meta-gnome layer, but 'x11' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-gnome README for details on enabling meta-gnome support.
Loading cache: 100% |###########################################################################################################################################################################################################################################| Time: 0:00:00
Loaded 3904 entries from dependency cache.
NOTE: /work/repo/smart/out/flypcb/../../device/flypcb/img/bui3xx-image.bb: Parsing config file /work/repo/smart/device/flypcb/flash/conf/fly.json########################################################################## | ETA: 0:00:00
NOTE: /work/repo/smart/out/flypcb/../../device/flypcb/img/bui3xx-image.bb: Found size 1048576 kbyte for bui3xx-image
NOTE: /work/repo/smart/out/flypcb/../../device/flypcb/img/bui3xx-image-remote-sysroot.bb: Parsing config file /work/repo/smart/device/flypcb/flash/conf/fly.json######################################################################## | ETA: 0:00:00
NOTE: /work/repo/smart/out/flypcb/../../device/flypcb/img/bui3xx-image-remote-sysroot.bb: Found size 1048576 kbyte for bui3xx-image
Parsing recipes: 100% |#########################################################################################################################################################################################################################################| Time: 0:00:05
Parsing of 2944 .bb files complete (2735 cached, 209 parsed). 4110 targets, 490 skipped, 2 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.42.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "fly"
DISTRO = "poky"
DISTRO_VERSION = "2.7.1"
TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky
meta-yocto-bsp = "HEAD:4686af030cf4933bde640322f1f1e254949f5739"
meta-bosch-build = "HEAD:81aa956ccfadb1aced1f9ccbfe834d4a3c94b7bd"
staging = "<unknown>:<unknown>"
meta-bui35x
meta-bui3xx-common = "HEAD:2316467e69cdc85922d89ea5492b0bf641096abd"
meta-freescale = "HEAD:6f1a07fa91caa73f6555565bf2012cc576c771bc"
meta-qt5 = "HEAD:5f99fc56b827e62ba4acee12f8d9164b75e164f2"
meta-clang = "HEAD:1f8d62ee6de51361a23316733a42d0dd4ca67390"
meta-java = "HEAD:2fc78571483465ca2fc69d6bd77632acd35e0770"
meta-oe
meta-python
meta-gnome
meta-multimedia
meta-webserver
meta-filesystems
meta-xfce
meta-networking = "HEAD:67b55a2b0750f31fc03908a823f05a8a152c54e3"

Initialising tasks: 100% |######################################################################################################################################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 8 Found 0 Missed 8 Current 78 (0% match, 90% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: make-mod-scripts-1.0-r0 do_configure: oe_runmake failed
ERROR: make-mod-scripts-1.0-r0 do_configure: Function failed: do_configure (log file is located at /work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/temp/log.do_configure.15772)
ERROR: Logfile of failure stored in: /work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/temp/log.do_configure.15772
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/gcc/gcc-runtime_8.3.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-bsp/u-boot/u-boot-tools_2019.01.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-core/glibc/glibc_2.29.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-kernel/kmod/kmod-native_git.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/bison/bison_3.0.4.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-support/lzop/lzop_1.04.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-extended/xz/xz_5.2.4.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/gcc/gcc-cross_8.3.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-connectivity/openssl/openssl_1.1.1b.bb:do_populate_sysroot', 'virtual:native:/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-extended/bc/bc_1.07.1.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot', '/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-devtools/binutils/binutils-cross_2.32.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['gcc-runtime', 'u-boot-tools-native', 'quilt-native', 'glibc', 'kmod-native', 'bison-native', 'lzop-native', 'pkgconfig-native', 'xz-native', 'gcc-cross-arm', 'openssl-native', 'bc-native', 'kern-tools-native', 'binutils-cross-arm', 'flex-native', 'linux-libc-headers', 'libtool-native', 'autoconf-native', 'gnu-config-native', 'automake-native', 'lzo-native', 'gmp-native', 'libmpc-native', 'texinfo-dummy-native', 'mpfr-native', 'zlib-native', 'readline-native', 'python3-native', 'gtk-doc-native', 'gettext-minimal-native', 'libgcc', 'm4-native', 'ncurses-native', 'libtirpc-native', 'libnsl2-native', 'libffi-native', 'sqlite3-native', 'bzip2-native', 'gdbm-native', 'util-linux-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_configure
| NOTE: make HOSTCC=gcc -isystem/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/usr/lib -L/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/lib -Wl,--enable-new-dtags -Wl,-rpath-link,/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/lib -Wl,-rpath,/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/work/repo/smart/out/flypcb/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 HOSTCPP=gcc -E CC=arm-poky-linux-gnueabi-gcc -mno-thumb-interwork -marm -fuse-ld=bfd -fmacro-prefix-map=/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0=/usr/src/debug/make-mod-scripts/1.0-r0 -fdebug-prefix-map=/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0=/usr/src/debug/make-mod-scripts/1.0-r0 -fdebug-prefix-map=/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot= -fdebug-prefix-map=/work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/recipe-sysroot-native= -fdebug-prefix-map=/work/repo/smart/out/flypcb/tmp/work-shared/fly/kernel-source=/usr/src/kernel LD=arm-poky-linux-gnueabi-ld.bfd AR=arm-poky-linux-gnueabi-ar -C /work/repo/smart/out/flypcb/tmp/work-shared/fly/kernel-source O=/work/repo/smart/out/flypcb/tmp/work-shared/fly/kernel-build-artifacts scripts prepare
| make: Entering directory '/work/repo/smart/os/linux-kernel'
| make[1]: Entering directory '/work/repo/smart/out/flypcb/tmp/work-shared/fly/kernel-build-artifacts'
| HOSTCC scripts/basic/fixdep
| GEN ./Makefile
| HOSTCC scripts/kconfig/conf.o
| SHIPPED scripts/kconfig/zconf.tab.c
| SHIPPED scripts/kconfig/zconf.lex.c
| HOSTCC scripts/kconfig/zconf.tab.o
| HOSTLD scripts/kconfig/conf
| scripts/kconfig/conf --silentoldconfig Kconfig
| ***
| *** Configuration file ".config" not found!
| ***
| *** Please run some configurator (e.g. "make oldconfig" or
| *** "make menuconfig" or "make xconfig").
| ***
| /work/repo/smart/os/linux-kernel/scripts/kconfig/Makefile:38: recipe for target 'silentoldconfig' failed
| make[3]: *** [silentoldconfig] Error 1
| /work/repo/smart/os/linux-kernel/Makefile:520: recipe for target 'silentoldconfig' failed
| make[2]: *** [silentoldconfig] Error 2
| make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'scripts'. Stop.
| make[1]: Leaving directory '/work/repo/smart/out/flypcb/tmp/work-shared/fly/kernel-build-artifacts'
| Makefile:146: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| make: Leaving directory '/work/repo/smart/os/linux-kernel'
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /work/repo/smart/out/flypcb/tmp/work/fly-poky-linux-gnueabi/make-mod-scripts/1.0-r0/temp/log.do_configure.15772)
ERROR: Task (/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-kernel/make-mod-scripts/make-mod-scripts_1.0.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 547 tasks of which 546 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/work/repo/smart/out/flypcb/../../build/yocto/poky/meta/recipes-kernel/make-mod-scripts/make-mod-scripts_1.0.bb:do_configure
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

ラベル(1)
0 件の賞賛
返信
1 返信

1,603件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ravicalm,

I hope you are doing well.

It seems that the kernel configuration file is dirty or it does not exist.

Please try running the below command before bitbake kernel-module-imx-gpu-viv.

bitbake -c menuconfig virtual/kernel.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信