[I.MX93] eMMC design : pull-up & pull-down resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[I.MX93] eMMC design : pull-up & pull-down resistor

ソリューションへジャンプ
1,400件の閲覧回数
Chou
Contributor II

Dear NXP Community,

I am currently working on the eMMC PCBA design for the I.MX93 and noticed some differences between the NXP EVK design and our initial design. I would like to seek clarification on this matter.

Based on the eMMC design guidelines I reviewed, it appears that pull-up resistors are generally required for CMD and DAT0-DAT7, and a pull-down resistor is needed for DS.

Chou_0-1738060316587.png
However, upon referencing your design in the SPF-94611_B1.pdf, I noticed that these additional external resistors are not present in the eMMC circuitry.

Chou_1-1738060352184.png

Could you kindly confirm if the absence of these external resistors is due to the presence of internal pull-up or pull-down resistors for DAT0-DAT7 and CMD within the I.MX93?

Chou_2-1738060378021.png

If this understanding is correct, could you also advise whether configuring the internal pull-up or pull-down settings appropriately in the software will be sufficient to meet the design requirements?

Chou_3-1738060397029.png

Thank you for your support, and I look forward to your guidance!

Best regards,
Howard 

タグ(2)
0 件の賞賛
返信
1 解決策
1,379件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Chou!
Thank you for contacting NXP Support!

 

in iMX93-EVK board we configure the internal pull up resistors in those pins,. but I recommend to put external pull-up resistors to guarantee the logical state.

 

This is a reference schematic

 

Chavira_0-1738086072091.png

 

The pull-up resistors are configured in u-boot device tree and maintain the configuration on Linux device tree

 

Best Regards!

Chavira

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,380件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Chou!
Thank you for contacting NXP Support!

 

in iMX93-EVK board we configure the internal pull up resistors in those pins,. but I recommend to put external pull-up resistors to guarantee the logical state.

 

This is a reference schematic

 

Chavira_0-1738086072091.png

 

The pull-up resistors are configured in u-boot device tree and maintain the configuration on Linux device tree

 

Best Regards!

Chavira

 

0 件の賞賛
返信