I.MX8QXP M4 core FreeRTOS Applications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8QXP M4 core FreeRTOS Applications

1,621件の閲覧回数
ajmalali
Contributor III

Hi,

I am using the 2.3 SDK (SDK_2.3_MEK-MIMX8QX_M4_Beta_Linux .run) for the development of some custom Applications. Is it possible to develop C++ applications in FreeRTOS? If yes what changes should i make in the build setup (build_debug.sh) for the SDK to support c++ applications?

Thank you for the support.

Regards,

Ajmal

0 件の賞賛
返信
1 返信

1,394件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

please look on

Using FreeRTOS with C++ – FreeRTOS Interactive 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信