I.MX8QXP M4 core FreeRTOS Applications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8QXP M4 core FreeRTOS Applications

1,665 Views
ajmalali
Contributor III

Hi,

I am using the 2.3 SDK (SDK_2.3_MEK-MIMX8QX_M4_Beta_Linux .run) for the development of some custom Applications. Is it possible to develop C++ applications in FreeRTOS? If yes what changes should i make in the build setup (build_debug.sh) for the SDK to support c++ applications?

Thank you for the support.

Regards,

Ajmal

0 Kudos
Reply
1 Reply

1,438 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

please look on

Using FreeRTOS with C++ – FreeRTOS Interactive 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply