I.MX8QMAX : bitbake fsl-image-qt5-validation-imx -c populate_sdk Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8QMAX : bitbake fsl-image-qt5-validation-imx -c populate_sdk Error

1,230件の閲覧回数
santhosh2
Contributor IV

Hi,

I have got below error when doing bitbake fsl-image-qt5-validation-imx -c populate_sdk


Computing transaction...error: Can't install packagegroup-core-ssh-dropbear-1.0-r1@all: it's locked


Please find the snap shot attached

populate_sdk.png

Let me know how to resolve this


Regards

Santhosh

0 件の賞賛
返信
2 返答(返信)

1,121件の閲覧回数
santhosh2
Contributor IV

Hi,

after comminting the below packages in local.conf file I am getting the error(please ref the screen shot)

#SSH
#PACKAGE_EXCLUDE += " packagegroup-core-ssh-dropbear"
#CORE_IMAGE_EXTRA_INSTALL += "openssh"

populate_sdk1.png

I tried below

bitbake -f fsl-image-qt5-validation-imx

bitbake fsl-image-qt5-validation-imx  -c populate_sdk

but still get the above error

Regards

Santhosh

0 件の賞賛
返信

1,121件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Santhosh Kumar, 

I'd like to try to reproduce this error. I would like to confirm the BSP you are using, is it the L4.9.51 BSP? Is it the GA or the Beta version? If it's the later it would make sense to switch to the GA in case this error was corrected. And also, are you following the Yocto Project User's Guide? Would you please share the setting (Distro, Machine) you are using?


Regards,

0 件の賞賛
返信