HI Igor,
So how do we ensure to give proper MAC address instead of setting the fake mac address in uboot, Please advice
I tried setting the MAC address randomly by enabling the below in imx8mm_evk.h file but same issue i got when i tried pining.
#define CONFIG_NET_RANDOM_ETHADDR
Please find the below trace
--------------------------------------------------------------------------------------
U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g7ade5b4 (Jun 12 2020 - 10:41:34 +0000)
CPU: Freescale i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 62C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
debug setup_fec
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
No panel detected: default to MIPI2HDMI
adv7535_init: Can't find device id=0x3d, on bus 1
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF d6451cc
- U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g7ade5b4
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:
Warning: ethernet@30be0000 (eth0) using random MAC address - 02:01:02:03:04:05
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
u-boot=>
--------------------------------------------------------------------------------------