[I.MX8M Plus] using DMA to do memory copy from RAM to RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[I.MX8M Plus] using DMA to do memory copy from RAM to RAM

Jump to solution
1,874 Views
linzhenggang1
Contributor II

Is it possible to do a RAM-to-RAM memory copy using DMA?

If yes, how should we do that in Linux?

P.S. We are using BSP L6.1.22

0 Kudos
Reply
1 Solution
1,752 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it's correct!, if you like to copy RAM to RAM can use the SDMA but The current drivers don't have the API to do it.

Regards

View solution in original post

0 Kudos
Reply
5 Replies
1,849 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it is possible, but you need to clarify which memory to what memory are you using, you can use the provided driver in the BSP.

Regards

0 Kudos
Reply
1,839 Views
linzhenggang1
Contributor II

Thank you for your reply.

Sorry, I don't understand the meaning of "which RAM and what RAM" you said.
I just want to do a memory copy in a user-space application(not from or to a peripheral) by using DMA to reduce my CPU usage.

If it is possible, could you please show me which part of the BSP I should use to do that?

Thank you very much!

0 Kudos
Reply
1,816 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no code to show how to use dma, but one can show the section 3.7.3 of the linux reference manual:

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards

 

0 Kudos
Reply
1,758 Views
linzhenggang1
Contributor II

Thank you for your reply.

In 3.7.1, it said that the SDMA API driver is for other drivers(kernel mode) but not for a user space application. Is my understanding correct?

---

3.7.1 Overview
The Smart Direct Memory Access (SDMA) API driver controls the SDMA hardware. It provides an API to other
drivers for transferring data between MCU memory space and the peripherals. It supports the following features:

0 Kudos
Reply
1,753 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it's correct!, if you like to copy RAM to RAM can use the SDMA but The current drivers don't have the API to do it.

Regards

0 Kudos
Reply