I.MX8 MINI MIPI DSI to HDMI is not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8 MINI MIPI DSI to HDMI is not working

ソリューションへジャンプ
4,090件の閲覧回数
bejanissim
Contributor I

Dear all,

My question refers to imx8 evk (8MMINILPD4-EVK).

I tried to connect an external HDMI display to the evk via the IMX-MIPI-HDMI converter (connect one side of the converter to DSI MIPI connector of the evk the it's other side to the HDMI display).

A pre-built image (imx-image-full-imx8mmevk.wic) from L5.4.47-2.2.0_images_MX8MMEVK.zip has been used.

When i turn on the evk i cannot see any image on the HDMI screen.

uboot and kernel informs that the driver of the video device cannot be loaded.

please advice, 

Nissim

Console output:

U-Boot SPL 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Sep 11 2020 - 22:00:22 +0000)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.2(release):imx_5.4.47_er2-2-gc949a888e
NOTICE: BL31: Built : 20:28:08, Sep 9 2020


U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Sep 11 2020 - 22:00:22 +0000)

CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 30C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

[*]-Video Link 0Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22

[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF c949a88
- U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5

Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Run CMD11 1.8V switch
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Run CMD11 1.8V switch
27941376 bytes read in 333 ms (80 MiB/s)
Booting from mmc ...
45394 bytes read in 15 ms (2.9 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300e151
Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.4.47-2.2.0+g5ec03d06f54e (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Thu Sep 24 09:14:28 UTC 2020
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000078000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbdbdc500-0xbdbddfff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000bdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507008
[ 0.000000] Policy zone: DMA32
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1336092K/2060288K available (16508K kernel code, 1238K rwdata, 6528K rodata, 2944K init, 1015K bss, 68836K reserved, 655360K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000374] Console: colour dummy device 80x25
[ 0.000437] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000446] pid_max: default: 32768 minimum: 301
[ 0.000512] LSM: Security Framework initializing
[ 0.000564] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.000575] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.024007] ASID allocator initialised with 32768 entries
[ 0.032004] rcu: Hierarchical SRCU implementation.
[ 0.040803] EFI services will not be available.
[ 0.048033] smp: Bringing up secondary CPUs ...
[ 0.080177] Detected VIPT I-cache on CPU1
[ 0.080201] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.080233] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.112207] Detected VIPT I-cache on CPU2
[ 0.112222] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.112240] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.144253] Detected VIPT I-cache on CPU3
[ 0.144270] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.144286] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.144340] smp: Brought up 1 node, 4 CPUs
[ 0.144363] SMP: Total of 4 processors activated.
[ 0.144369] CPU features: detected: 32-bit EL0 Support
[ 0.144376] CPU features: detected: CRC32 instructions
[ 0.151042] CPU: All CPU(s) started at EL2
[ 0.151061] alternatives: patching kernel code
[ 0.152490] devtmpfs: initialized
[ 0.158875] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.158892] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.174872] pinctrl core: initialized pinctrl subsystem
[ 0.175566] DMI not present or invalid.
[ 0.175810] NET: Registered protocol family 16
[ 0.190675] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.190704] audit: initializing netlink subsys (disabled)
[ 0.190937] audit: type=2000 audit(0.188:1): state=initialized audit_enabled=0 res=1
[ 0.191724] cpuidle: using governor menu
[ 0.192134] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.192946] Serial: AMBA PL011 UART driver
[ 0.193003] imx mu driver is registered.
[ 0.193022] imx rpmsg driver is registered.
[ 0.198709] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.221726] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.221737] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.221742] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.221749] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.222568] cryptd: max_cpu_qlen set to 1000
[ 0.225604] ACPI: Interpreter disabled.
[ 0.226511] iommu: Default domain type: Translated
[ 0.226649] vgaarb: loaded
[ 0.226954] SCSI subsystem initialized
[ 0.227268] usbcore: registered new interface driver usbfs
[ 0.227304] usbcore: registered new interface driver hub
[ 0.227354] usbcore: registered new device driver usb
[ 0.228532] mc: Linux media interface: v0.10
[ 0.228556] videodev: Linux video capture interface: v2.00
[ 0.228621] pps_core: LinuxPPS API ver. 1 registered
[ 0.228628] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.228639] PTP clock support registered
[ 0.228771] EDAC MC: Ver: 3.0.0
[ 0.229531] No BMan portals available!
[ 0.229751] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[ 0.230001] No QMan portals available!
[ 0.230376] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 0.230774] FPGA manager framework
[ 0.230849] Advanced Linux Sound Architecture Driver Initialized.
[ 0.231216] Bluetooth: Core ver 2.22
[ 0.231239] NET: Registered protocol family 31
[ 0.231243] Bluetooth: HCI device and connection manager initialized
[ 0.231252] Bluetooth: HCI socket layer initialized
[ 0.231258] Bluetooth: L2CAP socket layer initialized
[ 0.231270] Bluetooth: SCO socket layer initialized
[ 0.231936] clocksource: Switched to clocksource arch_sys_counter
[ 0.232086] VFS: Disk quotas dquot_6.6.0
[ 0.232134] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.232284] pnp: PnP ACPI: disabled
[ 0.237645] thermal_sys: Registered thermal governor 'step_wise'
[ 0.237648] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.237968] NET: Registered protocol family 2
[ 0.238277] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.238309] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.238416] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.238645] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.238720] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.238762] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.238892] NET: Registered protocol family 1
[ 0.239221] RPC: Registered named UNIX socket transport module.
[ 0.239226] RPC: Registered udp transport module.
[ 0.239230] RPC: Registered tcp transport module.
[ 0.239235] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.239593] PCI: CLS 0 bytes, default 64
[ 0.240414] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.240772] kvm [1]: IPA Size Limit: 40bits
[ 0.241355] kvm [1]: GICv3: no GICV resource entry
[ 0.241360] kvm [1]: disabling GICv2 emulation
[ 0.241377] kvm [1]: GIC system register CPU interface enabled
[ 0.241433] kvm [1]: vgic interrupt IRQ1
[ 0.241521] kvm [1]: Hyp mode initialized successfully
[ 0.244288] Initialise system trusted keyrings
[ 0.244394] workingset: timestamp_bits=44 max_order=19 bucket_order=0
[ 0.250097] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.250700] NFS: Registering the id_resolver key type
[ 0.250724] Key type id_resolver registered
[ 0.250728] Key type id_legacy registered
[ 0.250739] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.250756] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.251096] 9p: Installing v9fs 9p2000 file system support
[ 0.264512] Key type asymmetric registered
[ 0.264520] Asymmetric key parser 'x509' registered
[ 0.264553] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.264559] io scheduler mq-deadline registered
[ 0.264564] io scheduler kyber registered
[ 0.269837] EINJ: ACPI disabled.
[ 0.278560] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.278574] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.286492] mxs-dma 33000000.dma-controller: initialized
[ 0.287606] Bus freq driver module loaded
[ 0.292819] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.294933] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 5000000) is a IMX
[ 0.295389] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX
[ 0.295750] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX
[ 1.279955] printk: console [ttymxc1] enabled
[ 1.290433] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.297069] [drm] No driver support for vblank timestamp query.
[ 1.303061] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 1.312971] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 1.320536] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 1.328814] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -517
[ 1.345938] loop: module loaded
[ 1.351200] imx ahci driver is registered.
[ 1.358296] spi-nor spi3.0: n25q256ax1 (32768 Kbytes)
[ 1.369742] libphy: Fixed MDIO Bus: probed
[ 1.374612] tun: Universal TUN/TAP device driver, 1.6
[ 1.380434] thunder_xcv, ver 1.0
[ 1.383696] thunder_bgx, ver 1.0
[ 1.386965] nicpf, ver 1.0
[ 1.390500] pps pps0: new PPS source ptp0
[ 1.399709] libphy: fec_enet_mii_bus: probed
[ 1.405109] fec 30be0000.ethernet eth0: registered PHC device 0
[ 1.411647] Freescale FM module, FMD API version 21.1.0
[ 1.417135] Freescale FM Ports module
[ 1.420809] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 1.426534] fsl_dpa: FSL DPAA Ethernet driver
[ 1.431026] fsl_advanced: FSL DPAA Advanced drivers:
[ 1.436001] fsl_proxy: FSL DPAA Proxy initialization driver
[ 1.441686] fsl_oh: FSL FMan Offline Parsing port driver
[ 1.447846] hclge is initializing
[ 1.451174] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.458402] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.463776] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.470829] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.476609] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.482446] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.488402] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.495369] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.500984] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.508818] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.514906] sky2: driver version 1.30
[ 1.519505] VFIO - User Level meta-driver version: 0.3
[ 1.526438] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.532982] ehci-pci: EHCI PCI platform driver
[ 1.537501] ehci-platform: EHCI generic platform driver
[ 1.542914] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.549116] ohci-pci: OHCI PCI platform driver
[ 1.553600] ohci-platform: OHCI generic platform driver
[ 1.559518] usbcore: registered new interface driver uas
[ 1.564887] usbcore: registered new interface driver usb-storage
[ 1.570960] usbcore: registered new interface driver usbserial_generic
[ 1.577509] usbserial: USB Serial support registered for generic
[ 1.583544] usbcore: registered new interface driver ftdi_sio
[ 1.589313] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.596654] usbcore: registered new interface driver usb_serial_simple
[ 1.603205] usbserial: USB Serial support registered for carelink
[ 1.609320] usbserial: USB Serial support registered for zio
[ 1.615000] usbserial: USB Serial support registered for funsoft
[ 1.621028] usbserial: USB Serial support registered for flashloader
[ 1.627407] usbserial: USB Serial support registered for google
[ 1.633348] usbserial: USB Serial support registered for libtransistor
[ 1.639897] usbserial: USB Serial support registered for vivopay
[ 1.645927] usbserial: USB Serial support registered for moto_modem
[ 1.652214] usbserial: USB Serial support registered for motorola_tetra
[ 1.658849] usbserial: USB Serial support registered for novatel_gps
[ 1.665227] usbserial: USB Serial support registered for hp4x
[ 1.670993] usbserial: USB Serial support registered for suunto
[ 1.676933] usbserial: USB Serial support registered for siemens_mpi
[ 1.683318] usbcore: registered new interface driver usb_ehset_test
[ 1.691121] imx_usb 32e40000.usb: No over current polarity defined
[ 1.698599] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/soc@0:bus@30000000/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.713787] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.720075] i2c /dev entries driver
[ 1.724252] mx6s-csi 32e20000.csi1_bridge: initialising
[ 1.729993] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phy not found, using dummy regulator
[ 1.740179] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[ 1.747155] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[ 1.752837] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[ 1.766802] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0)
[ 1.773415] Bluetooth: HCI UART driver ver 2.3
[ 1.777873] Bluetooth: HCI UART protocol H4 registered
[ 1.783019] Bluetooth: HCI UART protocol BCSP registered
[ 1.788358] Bluetooth: HCI UART protocol LL registered
[ 1.793505] Bluetooth: HCI UART protocol ATH3K registered
[ 1.798929] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.805307] Bluetooth: HCI UART protocol Broadcom registered
[ 1.810993] Bluetooth: HCI UART protocol QCA registered
[ 1.818108] sdhci: Secure Digital Host Controller Interface driver
[ 1.824303] sdhci: Copyright(c) Pierre Ossman
[ 1.828858] Synopsys Designware Multimedia Card Interface Driver
[ 1.835446] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.841892] mmc0: CQHCI version 5.10
[ 1.845895] mmc1: CQHCI version 5.10
[ 1.849938] mmc2: CQHCI version 5.10
[ 1.885549] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 1.895690] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.902890] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)
[ 1.909614] caam 30900000.crypto: job rings = 2, qi = 0
[ 1.947578] caam algorithms registered in /proc/crypto
[ 1.953489] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto
[ 1.963019] caam_jr 30901000.jr: registering rng-caam
[ 1.968247] Device caam-keygen registered
[ 1.980712] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state
[ 1.989173] usbcore: registered new interface driver usbhid
[ 1.994769] usbhid: USB HID core driver
[ 2.000046] No fsl,qman node
[ 2.002932] Freescale USDPAA process driver
[ 2.007123] fsl-usdpaa: no region found
[ 2.010977] Freescale USDPAA process IRQ driver
[ 2.019067] optee: probing for conduit method from DT.
[ 2.024255] optee: revision 3.10 (b3914e54)
[ 2.025709] optee: dynamic shared memory is enabled
[ 2.035123] optee: initialized driver
[ 2.040085] galcore: clk_get vg clock failed, disable vg!
[ 2.045804] Galcore version 6.4.3.p0.286725
[ 2.088675] mmc2: Command Queue Engine enabled
[ 2.093200] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 2.100393] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 2.105060] mmcblk2boot0: mmc2:0001 DG4016 partition 1 4.00 MiB
[ 2.111130] mmcblk2boot1: mmc2:0001 DG4016 partition 2 4.00 MiB
[ 2.116643] hantrodec 0 : module inserted. Major = 236
[ 2.117747] mmcblk2rpmb: mmc2:0001 DG4016 partition 3 4.00 MiB, chardev (237:0)
[ 2.122724] hantrodec 1 : module inserted. Major = 236
[ 2.135552] hx280enc: module inserted. Major <235>
[ 2.138556] Alternate GPT is invalid, using primary GPT.
[ 2.144094] wm8524-codec audio-codec: Failed to get mute line: -517
[ 2.145735] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 2.194344] fsl-micfil-dai 30080000.micfil: GET IRQ: 16
[ 2.199604] fsl-micfil-dai 30080000.micfil: GET IRQ: 17
[ 2.204849] fsl-micfil-dai 30080000.micfil: GET IRQ: 18
[ 2.210094] fsl-micfil-dai 30080000.micfil: GET IRQ: 19
[ 2.220776] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 30090000.spdif mapping ok
[ 2.228384] imx-spdif sound-spdif: ASoC: no DMI vendor name!
[ 2.237184] imx-ak4458 sound-ak4458: ASoC: failed to init link ak4458: -517
[ 2.244179] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517)
[ 2.251531] debugfs: Directory '30080000.micfil' with parent 'imx-audio-micfil' already present!
[ 2.260410] imx-micfil sound-micfil: snd-soc-dummy-dai <-> 30080000.micfil mapping ok
[ 2.268261] imx-micfil sound-micfil: ASoC: no DMI vendor name!
[ 2.275886] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.286032] NET: Registered protocol family 26
[ 2.291043] NET: Registered protocol family 10
[ 2.296765] Segment Routing with IPv6
[ 2.300490] NET: Registered protocol family 17
[ 2.305643] Bluetooth: RFCOMM TTY layer initialized
[ 2.310535] Bluetooth: RFCOMM socket layer initialized
[ 2.315707] Bluetooth: RFCOMM ver 1.11
[ 2.319487] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.324806] Bluetooth: BNEP filters: protocol multicast
[ 2.330041] Bluetooth: BNEP socket layer initialized
[ 2.335012] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.340941] Bluetooth: HIDP socket layer initialized
[ 2.345948] 8021q: 802.1Q VLAN Support v1.8
[ 2.350155] lib80211: common routines for IEEE802.11 drivers
[ 2.355922] 9pnet: Installing 9P2000 support
[ 2.360226] tsn generic netlink module v1 init...
[ 2.364993] Key type dns_resolver registered
[ 2.370252] registered taskstats version 1
[ 2.374368] Loading compiled-in X.509 certificates
[ 2.399334] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 2.408157] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator
[ 2.438711] ldo6: supplied by regulator-dummy
[ 2.443858] i2c i2c-0: IMX I2C adapter registered
[ 2.449739] adv7511 1-003d: 1-003d supply avdd not found, using dummy regulator
[ 2.457123] adv7511 1-003d: 1-003d supply dvdd not found, using dummy regulator
[ 2.464471] adv7511 1-003d: 1-003d supply pvdd not found, using dummy regulator
[ 2.471838] adv7511 1-003d: 1-003d supply a2vdd not found, using dummy regulator
[ 2.479278] adv7511 1-003d: 1-003d supply v3p3 not found, using dummy regulator
[ 2.486634] adv7511 1-003d: 1-003d supply v1p2 not found, using dummy regulator
[ 2.494768] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e10000' disabled
[ 2.503915] i2c i2c-1: IMX I2C adapter registered
[ 2.511781] ak4458 2-0010: Failed to request supplies: -517
[ 2.517692] ak4458 2-0012: Failed to request supplies: -517
[ 2.523540] ak5558 2-0013: Failed to request supplies: -517
[ 2.529426] ak4458 2-0011: Failed to request supplies: -517
[ 2.535320] ov5640_mipi 2-003c: No sensor reset pin available
[ 2.541106] ov5640_mipi 2-003c: 2-003c supply DOVDD not found, using dummy regulator
[ 2.548908] ov5640_mipi 2-003c: 2-003c supply DVDD not found, using dummy regulator
[ 2.556606] ov5640_mipi 2-003c: 2-003c supply AVDD not found, using dummy regulator
[ 2.576245] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 2.581567] ov5640_mipi 2-003c: Camera is not found
[ 2.586633] i2c i2c-2: IMX I2C adapter registered
[ 2.593279] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator
[ 2.593323] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.602695] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.609067] [drm] No driver support for vblank timestamp query.
[ 2.620627] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 2.630514] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.638051] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 2.640302] imx6q-pcie 33800000.pcie: PCIe PLL locked after 20 us.
[ 2.646327] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 2.652545] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 2.660178] imx-drm soc@0:bus@32c00000:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.667409] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 2.677285] [drm] Initialized imx-drm 1.0.0 20120507 for soc@0:bus@32c00000:display-subsystem on minor 0
[ 2.684282] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 2.701881] imx_usb 32e40000.usb: No over current polarity defined
[ 2.708137] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator
[ 2.721462] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 2.733888] mmc0: CQHCI version 5.10
[ 2.768896] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.777102] mmc1: CQHCI version 5.10
[ 2.780755] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 2.791908] random: fast init done
[ 2.820768] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.830498] debugfs: Directory '30020000.sai' with parent 'bt-sco-audio' already present!
[ 2.838841] asoc-simple-card sound-bt-sco: bt-sco-pcm <-> 30020000.sai mapping ok
[ 2.846363] asoc-simple-card sound-bt-sco: ASoC: no DMI vendor name!
[ 2.852772] debugfs: File 'Playback' in directory 'dapm' already present!
[ 2.859590] debugfs: File 'Capture' in directory 'dapm' already present!
[ 2.868076] mmc0: queuing unknown CIS tuple 0x01 (3 bytes)
[ 2.874595] debugfs: Directory '30030000.sai' with parent 'wm8524-audio' already present!
[ 2.882914] asoc-simple-card sound-wm8524: wm8524-hifi <-> 30030000.sai mapping ok
[ 2.890559] asoc-simple-card sound-wm8524: ASoC: no DMI vendor name!
[ 2.904631] mmc0: queuing unknown CIS tuple 0x1a (5 bytes)
[ 2.910168] imx-ak4458 sound-ak4458: ASoC: failed to init link ak4458: -517
[ 2.917159] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517)
[ 2.926561] mmc0: queuing unknown CIS tuple 0x1b (8 bytes)
[ 2.932308] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 2.941046] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 2.949768] mmc0: queuing unknown CIS tuple 0x14 (0 bytes)
[ 2.972423] mmc0: queuing unknown CIS tuple 0x80 (1 bytes)
[ 2.977996] mmc0: queuing unknown CIS tuple 0x81 (1 bytes)
[ 2.983519] mmc0: queuing unknown CIS tuple 0x82 (1 bytes)
[ 2.989039] mmc0: new ultra high speed SDR104 SDIO card at address 0001
[ 3.306622] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.315077] ak4458 2-0010: ASoC: failed to probe component -6
[ 3.320868] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6
[ 3.327631] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6)
[ 3.338023] input: bd718xx-pwrkey as /devices/platform/soc@0/soc@0:bus@30800000/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input1
[ 3.351250] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:01 UTC (1)
[ 3.360693] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.372310] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.378909] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 3.386629] ALSA device list:
[ 3.387540] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 3.390508] #0: imx-spdif
[ 3.401063] #1: imx-audio-micfil
[ 3.404488] #2: bt-sco-audio
[ 3.407717] #3: wm8524-audio
[ 3.471067] mmc1: new ultra high speed SDR104 SDHC card at address 0001
[ 3.478791] mmcblk1: mmc1:0001 SD32G 29.1 GiB
[ 3.485724] mmcblk1: p1 p2
[ 3.685347] imx6q-pcie 33800000.pcie: Phy link never came up
[ 3.691051] imx6q-pcie 33800000.pcie: failed to initialize host
[ 3.696988] imx6q-pcie 33800000.pcie: unable to add pcie port.
[ 3.849699] EXT4-fs (mmcblk1p2): recovery complete
[ 3.855948] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.864099] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 3.872473] devtmpfs: mounted
[ 3.876243] Freeing unused kernel memory: 2944K
[ 3.880978] Run /sbin/init as init process
[ 4.033565] systemd[1]: System time before build time, advancing clock.
[ 4.057083] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 4.079029] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!

[ 4.125405] systemd[1]: Set hostname to <imx8mmevk>.
[ 4.306463] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus/system_bus_socket → /run/dbus/system_bus_socket; please update the unit file accordingly.
[ 4.334747] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslogd.pid → /run/syslogd.pid; please update the unit file accordingly.
[ 4.363682] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/rpcbind.sock → /run/rpcbind.sock; please update the unit file accordingly.
[ 4.387208] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/klogd.pid → /run/klogd.pid; please update the unit file accordingly.
[ 4.485262] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.492164] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 4.504565] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 4.515071] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.536103] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 4.556278] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Created slice User and Session Slice.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
[ OK ] Reached target Slices.
[ OK ] Reached target Swap.
[ OK ] Listening on Syslog Socket.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on udev Kernel Socket.
Mounting Huge Pages File System...
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
Starting Create list of st…odes for the current kernel...
Starting Journal Service...
Mounting Kernel Configuration File System...
Starting Remount Root and Kernel File Systems...
[ 4.937287] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
Starting Apply Kernel Variables...
Starting udev Coldplug all Devices...
Starting Setup Virtual Console...
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta… nodes for the current kernel.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Setup Virtual Console.
Starting Flush Journal to Persistent Storage...
[ 5.173079] systemd-journald[261]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Started udev Coldplug all Devices.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Start Psplash Boot Screen...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ 5.612098] Registered IR keymap rc-empty
[ OK [ 5.617310] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0
] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ 5.645435] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input2
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ 5.834211] qca9377: loading out-of-tree module taints kernel.
[ OK ] Started Job spooling tools.
Starting Console System Startup Logging...
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
Starting Packet Filtering Framework...
Starting Network Time Service (one-shot ntpdate mode)...
Starting Telephony service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started User Space Regulatory Firmware Loading.
Starting RPC Bind Service...
[ 6.043853] qca9377: loading driver v4.5.24.4
[ 6.048994] hifDeviceInserted: Dumping clocks (50000000,400000000)
[ 6.055498] AR6000: Set async interrupt delay clock as 2.
[ OK ] Started User Space SDMA Firmware Loading.
Starting System Logging Service...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started Console System Startup Logging.
[ OK ] Started Packet Filte[ 6.152300] imx-sdma 302b0000.dma-controller: loaded firmware 4.5
ring Framework.
[ OK ] Started Network Time Service (one-shot ntpdate mode).
[ OK ] Started RPC Bind Service.
[ 6.204864] AR6000: configuration opcode 3 is not used for Linux SDIO stack
[ OK ] [ 6.221049] NUM_DEV=1 FWMODE=0x2 FWSUBMODE=0x0 FWBR_BUF 0
Started System Logging Service.
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Created slice system-weston.slice.
[ OK ] Reached target Network (Pre).
Starting Save/Restore Sound Card State...
Starting Connection service...
Starting Kernel Logging Service...
Starting Network Service...
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ OK ] Started Network Service.
[ 6.664340] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL)
[ OK ] Started Connection service.
Starting Avahi mDNS/DNS-SD Stack...
Starting Hostname Service...
[ 6.775265] HIF Interrupt processing is SYNC ONLY
[ 6.780758] AR6000: configuration opcode 7 is only used for RTOS systems, not Linux systems
Starting WPA supplicant...
[ 6.794739] AR6000: configuration opcode 5 is not used for Linux SDIO stack
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Created slice system[ 6.882954] +HWT
-systemd\x2dfsck.slice.
[ OK ] Started 6.905378] -HWT
;39mWPA supplicant.
[ 6.915250] MAILBOX SWAP Service is enabled!
[ OK ] Started Kernel Logging Service.
[ 6.929986] Reduced Tx Complete service is enabled!
[ 6.941209] HTCConnectService, host indicate support b2b bundle
[ OK ] Found device /dev/mmcblk2p12.
[ 6.969012] HTCConnectService, firmware decide to disabled b2b bundle
[ OK ] Started Hostname Service.
[ 6.980455] HTC Service:0x0300 ep:1 TX flow control disabled
[ OK ] Reached target Netwo[ 6.995326] HTCConnectService, host indicate support b2b bundle
rk.
[ 7.006330] HTCConnectService, firmware decide to disabled b2b bundle
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started 7.041272] target uses HTT version 3.53; host uses 3.28
;39mUpdate psplash to network.
[ 7.052086] Host SW:4.5.24.4, FW:0.0.0.23, HW:QCA93x7_REV1_1
Starting Terminate Psplash Boot Screen...
[ 7.075672] ol_pktlog_init: pktlogmod_init successfull
Starting /etc/rc.local Compatibility...
[ 7.103717] ath_hif_sdio: HIF (Atheros/multi-bss)
Starting File System Check on /dev/mmcblk2p12 qca9377: driver loaded in 1076000
[0m...
Starting Permit User Sessions...
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Started Permit User Sessions.
[ OK ] Started File System Check on /dev/mmcblk2p12.
Mounting /run/media/mmcblk2p12...
[ OK ] [ 7.385098] EXT4-fs (mmcblk2p12): The kernel was not built with CONFIG_QUOTA and CONFIG_QFMT_V2
Started Getty on tty1.
[ OK ] Started Serial Getty on ttymxc1.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting File System Check on /dev/mmcblk1p1...
Starting File System Check on /dev/mmcblk2p10...
Starting File System Check on /dev/mmcblk2p11...
Starting File System Check on /dev/mmcblk2p5...
Starting File System Check on /dev/mmcblk2p6...
Starting Update UTMP about System Runlevel Changes...
Starting Weston Wayland Compositor (on tty7)...
[FAILED] Failed to mount /run/media/mmcblk2p12.
See 'systemctl status run-media-mmcblk2p12.mount' for details.
[ OK ] Started Weston Wayland Compositor (on tty7).
[ OK ] Started Update UTMP about System Runlevel Changes.
[ OK ] Started File System Check on /dev/mmcblk1p1.
Mounting /run/media/mmcblk1p1...
[ OK ] Mounted /run/media/mmcblk1p1.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 7.711185] audit: type=1006 audit(1597849393.672:2): pid=840 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ OK ] Started File System Check on /dev/mmcblk2p11.
Mounting /run/media/mmcblk2p11...
[ OK ] Started File System Check on /dev/mmcblk2p10.
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of user root.
Mounting /run/media/mmcblk2p10...
[ 8.213325] EXT4-fs (mmcblk2p11): mounted filesystem without journal. Opts: (null)
[ 8.228079] ext4 filesystem being mounted at /run/media/mmcblk2p11 supports timestamps until 2038 (0x7fffffff)
[ 8.239224] EXT4-fs (mmcblk2p10): mounted filesystem without journal. Opts: (null)
[ 8.247545] ext4 filesystem being mounted at /run/media/mmcblk2p10 supports timestamps until 2038 (0x7fffffff)
[ OK ] Mounted /run/media/mmcblk2p11.
[ OK ] Mounted /run/media/mmcblk2p10.
[ OK ] Started File System Check on /dev/mmcblk2p5.
[ OK ] Started File System Check on /dev/mmcblk2p6.
Mounting /run/media/mmcblk2p5...
[ 8.678453] EXT4-fs (mmcblk2p5): mounted filesystem without journal. Opts: (null)
Mounting /run/media/mmcblk2p6...
[ 8.697998] EXT4-fs (mmcblk2p6): mounted filesystem without journal. Opts: (null)
[ OK ] Mounted /run/media/mmcblk2p5.
[ OK ] Mounted /run/media/mmcblk2p6.
[ 10.487965] random: crng init done
[ 10.491376] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.

NXP i.MX Release Distro 5.4-zeus imx8mmevk ttymxc1

imx8mmevk login:

 

 

0 件の賞賛
返信
1 解決策
4,074件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I just tested and it was fine.Please check that display have independent power supply.

 

BR

Zhiming

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,075件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

I just tested and it was fine.Please check that display have independent power supply.

 

BR

Zhiming

0 件の賞賛
返信