I.MX6Q USB device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q USB device

1,412 Views
richarddestiny
Contributor III

Hi,all

        I‘m working in  I.MX6Q  SABREASD   kernel:3.10.17

        I want to  enumerate emmc  through  IMX6Q USB device as a  USB  falsh disk ,how to do  it?

thanks for you reply

have a great day!

Richard

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,265 Views
igorpadykov
NXP Employee
NXP Employee

HI Richard

one can look at unit tests mxc_usb_test and description in

doc folder : FSL-UT-USB-004.txt

Index of /buildsources/i/imx-test/imx-test-3.10.17-1.0.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply