Dear All,
I have I.MX6Q Sabre Automative Infoteinment card. It has UART, power and some other signals on CN1 connector on its base board. I want to connect a GPS device which has PPS signal to it. Where should I connect PPS signal?
RS232 DCD and DTR signals do not exist on this connector.
There is only "GPS_INTERR_B" signal which might be suitable. What is this signal's function?
Thank you,
Dear Victor,
Thank you so much,
Since I do not know very much about Linux kernel, I need additional information. How can I use this code? Should it be patched to the kernel?
You can refer this common recommendations regarding to driving PPS with GPIO pin:
http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/pps/pps-gpio.txt
http://www.linuxpps.org/pipermail/discussions/2013-April/004423.html
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------