I.MX6Q SABRE AUTOMATIVE GPS PPS CONNECTION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q SABRE AUTOMATIVE GPS PPS CONNECTION

1,074件の閲覧回数
neavyseal
Contributor I

Dear All,

I have I.MX6Q Sabre Automative Infoteinment card. It has UART, power and some other signals on CN1 connector on its base board. I want to connect a GPS device which has PPS signal to it. Where should I connect PPS signal?

RS232 DCD and DTR signals do not exist on this connector.

There is only "GPS_INTERR_B" signal which might be suitable. What is this signal's function?

Thank you,

0 件の賞賛
返信
2 返答(返信)

778件の閲覧回数
neavyseal
Contributor I

Dear Victor,

Thank you so much,

Since I do not know very much about Linux kernel, I need additional information. How can I use this code? Should it be patched to the kernel?

0 件の賞賛
返信

778件の閲覧回数
b36401
NXP Employee
NXP Employee

You can refer this common recommendations regarding to driving PPS with GPIO pin:

http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/pps/pps-gpio.txt
http://www.linuxpps.org/pipermail/discussions/2013-April/004423.html

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信