I.MX6Q Power on caton LOG!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q Power on caton LOG!

1,958 Views
tommyduan
Contributor III

     For the machine we have recently produced, we use IMX6Q chip, and found that after the first computer burning software, some machines cannot enter the menu after starting up, but caton the LOG of starting up is in the attachment, and the print information is in the attachment, please help to analyze it! If I use the computer to burn software again, it will be ok!

Labels (1)
0 Kudos
Reply
3 Replies

1,843 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   As I understand, if the system is re-written on the boot media, the first boot is correct.

Is it possible to look at the correct boot log?

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

1,843 Views
tommyduan
Contributor III

Thanks  for your replay!I sent "recovery"commmand,the caton log is ok

What might be the reason from the previous abnormal LOG?

!Here is the log of the normal boot:

(190605_10:05:46.146)U-Boot 2015.04-g4f3a24b-dirty (Jan 10 2019 - 21:14:50), Build: jenkins-android platform-SYS CNE-6535B-D-138
(190605_10:05:46.146)CPU: Freescale i.MX6Q rev1.5 at 792 MHz
(190605_10:05:46.146)Reset cause: POR
(190605_10:05:46.146)DRAM: 2 GiB
(190605_10:05:46.522)Starting kernel ...
(190605_10:05:47.456)Linux version 4.1.15-g2a34798-dirty (jenkins9@yb-android2) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #1 SMP PREEMPT Thu Jan 10 21:15:58 CST 2019
(190605_10:05:47.456)Kernel command line: console=ttymxc0,921600 usbcore.autosuspend=-1 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled androidboot.serialno=1f1769d4ee6ba68e
(190605_10:05:49.828)root@sabresd_6dq:/ #
(190605_10:05:54.211)cat /proc/kmsg
(190605_10:05:54.275)<6>Booting Linux on physical CPU 0x0
(190605_10:05:54.275)<6>Initializing cgroup subsys cpu
(190605_10:05:54.275)<6>Initializing cgroup subsys cpuacct
(190605_10:05:54.275)<2>Linux version 4.1.15-g2a34798-dirty (jenkins9@yb-android2) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #1 SMP PREEMPT Thu Jan 10 21:15:58 CST 2019
(190605_10:05:54.275)<6>CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
(190605_10:05:54.275)<6>CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
(190605_10:05:54.275)<6>Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
(190605_10:05:54.275)<6>cma: Reserved 384 MiB at 0x26000000
(190605_10:05:54.275)<6>Memory policy: Data cache writealloc
(190605_10:05:54.275)<7>On node 0 totalpages: 524032
(190605_10:05:54.275)<7>free_area_init_node: node 0, pgdat c0c6e380, node_mem_map d5000000
(190605_10:05:54.275)<7> Normal zone: 1504 pages used for memmap
(190605_10:05:54.275)<7> Normal zone: 0 pages reserved
(190605_10:05:54.275)<7> Normal zone: 192512 pages, LIFO batch:31
(190605_10:05:54.275)<7> HighMem zone: 331520 pages, LIFO batch:31
(190605_10:05:54.275)<6>PERCPU: Embedded 13 pages/cpu @eeede000 s21248 r8192 d23808 u53248
(190605_10:05:54.275)<7>pcpu-alloc: s21248 r8192 d23808 u53248 alloc=13*4096
(190605_10:05:54.275)<7>pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
(190605_10:05:54.275)<6>Built 1 zonelists in Zone order, mobility grouping on. Total pages: 522528
(190605_10:05:54.275)<2>Kernel command line: console=ttymxc0,921600 usbcore.autosuspend=-1 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled androidboot.serialno=1f1769d4ee6ba68e
(190605_10:05:54.275)<6>PID hash table entries: 4096 (order: 2, 16384 bytes)
(190605_10:05:54.275)<6>Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
(190605_10:05:54.275)<6>Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
(190605_10:05:54.275)<6>Memory: 345112K/2096128K available (7381K kernel code, 462K rwdata, 2388K rodata, 1024K init, 596K bss, 1357800K reserved, 393216K cma-reserved, 0K highmem)
(190605_10:05:54.275)<5>Virtual kernel memory layout:
(190605_10:05:54.275)<5> vector : 0xffff0000 - 0xffff1000 ( 4 kB)
(190605_10:05:54.275)<5> fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
(190605_10:05:54.275)<5> vmalloc : 0xef800000 - 0xff000000 ( 248 MB)
(190605_10:05:54.275)<5> lowmem : 0xc0000000 - 0xef000000 ( 752 MB)
(190605_10:05:54.275)<5> pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
(190605_10:05:54.275)<5> modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
(190605_10:05:54.275)<5> .text : 0xc0008000 - 0xc0a8a78c (10762 kB)
(190605_10:05:54.275)<5> .init : 0xc0b00000 - 0xc0c00000 (1024 kB)
(190605_10:05:54.275)<5> .data : 0xc0c00000 - 0xc0c73938 ( 463 kB)
(190605_10:05:54.275)<5> .bss : 0xc0c73938 - 0xc0d08a4c ( 597 kB)
(190605_10:05:54.275)<6>SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
(190605_10:05:54.275)<6>Preemptible hierarchical RCU implementation.
(190605_10:05:54.275)<6> Additional per-CPU info printed with stalls.
(190605_10:05:54.275)<6>NR_IRQS:16 nr_irqs:16 16
(190605_10:05:54.275)<6>L2C-310 erratum 769419 enabled
(190605_10:05:54.275)<6>L2C-310 enabling early BRESP for Cortex-A9
(190605_10:05:54.275)<6>L2C-310 full line of zeros enabled for Cortex-A9
(190605_10:05:54.275)<6>L2C-310 ID prefetch enabled, offset 16 lines
(190605_10:05:54.275)<6>L2C-310 dynamic clock gating enabled, standby mode enabled
(190605_10:05:54.275)<6>L2C-310 cache controller enabled, 16 ways, 1024 kB
(190605_10:05:54.275)<6>L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001
(190605_10:05:54.276)<6>mxc_clocksource_init 3000000
(190605_10:05:54.276)<6>Switching to timer-based delay loop, resolution 333ns
(190605_10:05:54.276)<6>sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
(190605_10:05:54.276)<6>clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
(190605_10:05:54.276)<6>Console: colour dummy device 80x30
(190605_10:05:54.276)<6>Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
(190605_10:05:54.276)<6>pid_max: default: 32768 minimum: 301
(190605_10:05:54.276)<6>Security Framework initialized
(190605_10:05:54.276)<6>SELinux: Initializing.
(190605_10:05:54.276)<7>SELinux: Starting in permissive mode
(190605_10:05:54.276)<6>AppArmor: AppArmor disabled by boot time parameter
(190605_10:05:54.276)<6>Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
(190605_10:05:54.276)<6>Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
(190605_10:05:54.276)<6>Initializing cgroup subsys freezer
(190605_10:05:54.276)<6>Initializing cgroup subsys debug
(190605_10:05:54.276)<6>CPU: Testing write buffer coherency: ok
(190605_10:05:54.276)<7>create_sysfs_defer_highmem : register sysfs SUCCES
(190605_10:05:54.276)<6>CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
(190605_10:05:54.276)<6>Setting up static identity map for 0x10100000 - 0x10100058
(190605_10:05:54.276)<6>CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
(190605_10:05:54.276)<6>CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
(190605_10:05:54.276)<6>CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
(190605_10:05:54.276)<6>Brought up 4 CPUs
(190605_10:05:54.276)<6>SMP: Total of 4 processors activated (24.00 BogoMIPS).
(190605_10:05:54.276)<6>CPU: All CPU(s) started in SVC mode.
(190605_10:05:54.276)<6>devtmpfs: initialized
(190605_10:05:54.276)<6>VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
(190605_10:05:54.276)<6>clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
(190605_10:05:54.276)<6>pinctrl core: initialized pinctrl subsystem
(190605_10:05:54.276)<6>NET: Registered protocol family 16
(190605_10:05:54.276)<6>DMA: preallocated 256 KiB pool for atomic coherent allocations
(190605_10:05:54.276)<6>CPU identified as i.MX6Q, silicon rev 1.5
(190605_10:05:54.337)<4>!!request miniPCIE Power On gpio
(190605_10:05:54.340)<6>hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
(190605_10:05:54.340)<6>hw-breakpoint: maximum watchpoint size is 4 bytes.
(190605_10:05:54.340)<3>VDSO is not a valid ELF object!
(190605_10:05:54.340)<6>imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
(190605_10:05:54.340)<6>mxs-dma 110000.dma-apbh: initialized
(190605_10:05:54.340)<3>MPCIE_3V3: Failed to request enable GPIO83: -16
(190605_10:05:54.340)<3>reg-fixed-voltage regulators:regulator@3: Failed to register regulator: -16
(190605_10:05:54.340)<4>reg-fixed-voltage: probe of regulators:regulator@3 failed with error -16
(190605_10:05:54.340)<5>SCSI subsystem initialized
(190605_10:05:54.340)<7>libata version 3.00 loaded.
(190605_10:05:54.340)<6>i2c i2c-0: IMX I2C adapter registered
(190605_10:05:54.340)<6>i2c i2c-0: can't use DMA
(190605_10:05:54.340)<6>i2c i2c-1: IMX I2C adapter registered
(190605_10:05:54.340)<6>i2c i2c-1: can't use DMA
(190605_10:05:54.340)<6>i2c i2c-2: IMX I2C adapter registered
(190605_10:05:54.340)<6>i2c i2c-2: can't use DMA
(190605_10:05:54.340)<6>Linux video capture interface: v2.00
(190605_10:05:54.340)<6>usbcore: registered new interface driver usbfs
(190605_10:05:54.340)<6>usbcore: registered new interface driver hub
(190605_10:05:54.340)<6>usbcore: registered new device driver usb
(190605_10:05:54.340)<6>imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
(190605_10:05:54.340)<6>imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
(190605_10:05:54.340)<6>mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
(190605_10:05:54.340)<6>mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
(190605_10:05:54.340)<6>MIPI CSI2 driver module loaded
(190605_10:05:54.340)<6>Advanced Linux Sound Architecture Driver Initialized.
(190605_10:05:54.340)<6>Switched to clocksource mxc_timer1
(190605_10:05:54.340)<6>NET: Registered protocol family 2
(190605_10:05:54.340)<6>TCP established hash table entries: 8192 (order: 3, 32768 bytes)
(190605_10:05:54.340)<6>TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
(190605_10:05:54.341)<6>TCP: Hash tables configured (established 8192 bind 8192)
(190605_10:05:54.341)<6>UDP hash table entries: 512 (order: 2, 16384 bytes)
(190605_10:05:54.341)<6>UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
(190605_10:05:54.341)<6>NET: Registered protocol family 1
(190605_10:05:54.341)<6>Trying to unpack rootfs image as initramfs...
(190605_10:05:54.341)<6>Freeing initrd memory: 1012K (c5000000 - c50fd000)
(190605_10:05:54.341)<4>CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
(190605_10:05:54.341)<6>hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
(190605_10:05:54.341)<6>Bus freq driver module loaded
(190605_10:05:54.341)<6>console [pstore-1] enabled
(190605_10:05:54.341)<6>pstore: Registered ramoops as persistent store backend
(190605_10:05:54.341)<6>ramoops: attached 0x100000@0x8bf00000, ecc: 0/0
(190605_10:05:54.341)<6>mxc_ramoops device success loaded
(190605_10:05:54.341)<6>futex hash table entries: 1024 (order: 4, 65536 bytes)
(190605_10:05:54.341)<6>audit: initializing netlink subsys (disabled)
(190605_10:05:54.341)<5>audit: type=2000 audit(0.360:1): initialized
(190605_10:05:54.341)<6>fuse init (API version 7.23)
(190605_10:05:54.341)<7>SELinux: Registering netfilter hooks
(190605_10:05:54.341)<6>bounce: pool size: 64 pages
(190605_10:05:54.341)<6>io scheduler noop registered
(190605_10:05:54.341)<6>io scheduler deadline registered
(190605_10:05:54.341)<6>io scheduler cfq registered (default)
(190605_10:05:54.341)<6>imx-weim 21b8000.weim: Driver registered.
(190605_10:05:54.341)<4>+++++++++++++++++imx6_gpio_init_module OK2
(190605_10:05:54.341)<4>request micgpio 186
(190605_10:05:54.341)<4>request GPSgpio 87
(190605_10:05:54.341)<4>request SABRESD_DENOISE_RESET 67
(190605_10:05:54.341)<6>mxc_sdc_fb fb@0: registered mxc display driver ldb
(190605_10:05:54.341)<6>Console: switching to colour frame buffer device 100x30
(190605_10:05:54.341)<3>mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
(190605_10:05:54.341)<3>mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
(190605_10:05:54.341)<3>mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
(190605_10:05:54.341)<4>imx-sdma 20ec000.sdma: no iram assigned, using external mem
(190605_10:05:54.341)<4>imx-sdma 20ec000.sdma: no event needs to be remapped
(190605_10:05:54.341)<6>imx-sdma 20ec000.sdma: loaded firmware 3.3
(190605_10:05:54.341)<6>imx-sdma 20ec000.sdma: initialized
(190605_10:05:54.341)<6>2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 23, base_baud = 5000000) is a IMX
(190605_10:05:54.341)<6>console [ttymxc0] enabled
(190605_10:05:54.341)<6>21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 293, base_baud = 5000000) is a IMX
(190605_10:05:54.341)<6>21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 294, base_baud = 5000000) is a IMX
(190605_10:05:54.341)<6>21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 295, base_baud = 5000000) is a IMX
(190605_10:05:54.341)<6>21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 296, base_baud = 5000000) is a IMX
(190605_10:05:54.341)<6>[drm] Initialized drm 1.1.0 20060810
(190605_10:05:54.341)<6>[drm] Initialized vivante 1.0.0 20120216 on minor 0
(190605_10:05:54.341)<6>brd: module loaded
(190605_10:05:54.341)<6>loop: module loaded
(190605_10:05:54.341)<6>zram: Created 1 device(s)
(190605_10:05:54.341)<6>spi_imx 200c000.ecspi: probed
(190605_10:05:54.341)<6>spi_imx 2010000.ecspi: probed
(190605_10:05:54.341)<6>tun: Universal TUN/TAP device driver, 1.6
(190605_10:05:54.341)<6>tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
(190605_10:05:54.341)<6>PPP generic driver version 2.4.2
(190605_10:05:54.341)<6>PPP BSD Compression module registered
(190605_10:05:54.341)<6>PPP Deflate Compression module registered
(190605_10:05:54.341)<6>PPP MPPE Compression module registered
(190605_10:05:54.341)<6>NET: Registered protocol family 24
(190605_10:05:54.341)<6>usbcore: registered new interface driver cdc_ether
(190605_10:05:54.341)<6>usbcore: registered new interface driver cdc_eem
(190605_10:05:54.341)<6>usbcore: registered new interface driver cdc_subset
(190605_10:05:54.341)<6>usbcore: registered new interface driver cdc_ncm
(190605_10:05:54.342)<6>snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
(190605_10:05:54.342)<6>i2c /dev entries driver
(190605_10:05:54.342)<4>isl7998x is found, chip id reg 0x00 = 0x87.
(190605_10:05:54.342)<6>mxc_mipi_csi2 21dc000.mipi_csi: mipi_csi2_reset: mipi_lane_bps = 432 Mbps
(190605_10:05:54.342)<6>mxc_mipi_csi2 21dc000.mipi_csi: mipi_csi2_reset: value = 0xc.
(190605_10:05:54.342)<4>open backlight count=1 (ret=0):0x72 0x1 0x9
(190605_10:05:54.342)<4>@@@@@ set_brightness_contrast_saturation->rd_camera_para start
(190605_10:05:54.342)<7>camera para(0):0x72 0x1 0x8 0x0 0xa 0xa 0xa 0x1 0x1f
(190605_10:05:54.342)<4>@@@@@ set_brightness_contrast_saturation->rd_camera_para end
(190605_10:05:54.342)<4>@@@@@ set_brightness_contrast_saturation out
(190605_10:05:54.342)<6>isl7998x_mipi is found
(190605_10:05:54.342)<6>usbcore: registered new interface driver uvcvideo
(190605_10:05:54.342)<6>USB Video Class driver (1.1.1)
(190605_10:05:54.342)<6>ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
(190605_10:05:54.342)<6>usbcore: registered new interface driver cdc_acm
(190605_10:05:54.342)<6>cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
(190605_10:05:54.342)<6>usbcore: registered new interface driver usb-storage
(190605_10:05:54.342)<4>2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
(190605_10:05:54.342)<4>2184000.usb supply vbus not found, using dummy regulator
(190605_10:05:54.342)<4>@@@@@@@@@@@@@@ otgci = 0xd2038010
(190605_10:05:54.342)<4>@@@@@@@@@@@@@@ export usb power gpio
(190605_10:05:54.342)<4>2184200.usb supply vbus not found, using dummy regulator
(190605_10:05:54.342)<6>ci_hdrc ci_hdrc.1: EHCI Host Controller
(190605_10:05:54.398)<6>ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
(190605_10:05:54.400)<6>ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
(190605_10:05:54.400)<6>usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
(190605_10:05:54.400)<6>usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
(190605_10:05:54.400)<6>usb usb1: Product: EHCI Host Controller
(190605_10:05:54.400)<6>usb usb1: Manufacturer: Linux 4.1.15-g2a34798-dirty ehci_hcd
(190605_10:05:54.400)<6>usb usb1: SerialNumber: ci_hdrc.1
(190605_10:05:54.400)<6>hub 1-0:1.0: USB hub found
(190605_10:05:54.400)<6>hub 1-0:1.0: 1 port detected
(190605_10:05:54.400)<7>userial_init: registered 4 ttyGS* devices
(190605_10:05:54.400)<6>mousedev: PS/2 mouse device common for all mice
(190605_10:05:54.400)<6>usbcore: registered new interface driver usb_acecad
(190605_10:05:54.400)<6>usbcore: registered new interface driver aiptek
(190605_10:05:54.400)<6>usbcore: registered new interface driver gtco
(190605_10:05:54.401)<6>usbcore: registered new interface driver hanwang
(190605_10:05:54.401)<6>usbcore: registered new interface driver kbtab
(190605_10:05:54.401)<6>imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
(190605_10:05:54.401)<6>sdhci: Secure Digital Host Controller Interface driver
(190605_10:05:54.401)<6>sdhci: Copyright(c) Pierre Ossman
(190605_10:05:54.401)<6>sdhci-pltfm: SDHCI platform and OF driver helper
(190605_10:05:54.401)<6>/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
(190605_10:05:54.401)<6>sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
(190605_10:05:54.401)<6>sdhci-esdhc-imx 2198000.usdhc: assigned as wifi host
(190605_10:05:54.401)<6>sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
(190605_10:05:54.401)<6>sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
(190605_10:05:54.401)<6>mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
(190605_10:05:54.401)<6>/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
(190605_10:05:54.401)<6>sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
(190605_10:05:54.401)<6>sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
(190605_10:05:54.401)<6>mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
(190605_10:05:54.401)<6>mxc_vpu 2040000.vpu_fsl: VPU initialized
(190605_10:05:54.401)<6>mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
(190605_10:05:54.401)<6>Galcore version 5.0.11.41671
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x01 (3 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x1a (5 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x1b (8 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x14 (0 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x80 (1 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x81 (1 bytes)
(190605_10:05:54.401)<4>mmc2: queuing unknown CIS tuple 0x82 (1 bytes)
(190605_10:05:54.401)<6>mmc2: new high speed SDIO card at address 0001
(190605_10:05:54.401)<6>mmc3: MAN_BKOPS_EN bit is not set
(190605_10:05:54.401)<6>mmc3: new DDR MMC card at address 0001
(190605_10:05:54.401)<6>mmcblk3: mmc3:0001 PHIODM 14.5 GiB
(190605_10:05:54.401)<6>mmcblk3boot0: mmc3:0001 PHIODM partition 1 4.00 MiB
(190605_10:05:54.401)<6>mmcblk3boot1: mmc3:0001 PHIODM partition 2 4.00 MiB
(190605_10:05:54.401)<6>mmcblk3rpmb: mmc3:0001 PHIODM partition 3 4.00 MiB
(190605_10:05:54.401)<6> mmcblk3: p1 p2 p3 < p5 p6 p7 p8 p9 p10 > p4
(190605_10:05:54.401)<6>usb 1-1: new high-speed USB device number 2 using ci_hdrc
(190605_10:05:54.401)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.401)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.401)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.401)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.401)<6>usb 1-1: USB disconnect, device number 2
(190605_10:05:54.401)<6>usb 1-1: new high-speed USB device number 3 using ci_hdrc
(190605_10:05:54.401)<6>hidraw: raw HID events driver (C) Jiri Kosina
(190605_10:05:54.401)<6>usbcore: registered new interface driver usbhid
(190605_10:05:54.401)<6>usbhid: USB HID core driver
(190605_10:05:54.401)<6>ashmem: initialized
(190605_10:05:54.401)<6>usbcore: registered new interface driver snd-usb-audio
(190605_10:05:54.401)<4>+++CS42L52 Device ID (0)
(190605_10:05:54.401)<6>cs42l52 2-004a: Cirrus Logic CS42L52, Revision: 00
(190605_10:05:54.401)<4>+++navi Device ID (0)
(190605_10:05:54.401)<6>navi 2-002a: Cirrus Logic navi, Revision: 00
(190605_10:05:54.401)<4>cs42l52_probe
(190605_10:05:54.401)<6>imx-cs42l52 sound: cs42l52 <-> 202c000.ssi mapping ok
(190605_10:05:54.401)<3>imx-cs42l52 sound: ASoC: no source widget found for HPOUTL
(190605_10:05:54.401)<3>imx-cs42l52 sound: ASoC: Failed to add route HPOUTL -> direct -> Headphone Jack
(190605_10:05:54.401)<4>imx_cs42l52_late_probe
(190605_10:05:54.401)<3>cs42l52 2-004a: Unable to sync registers 0x2-0x6. -5
(190605_10:05:54.401)<4>navi_probe
(190605_10:05:54.401)<6>imx-navi sound1: navi <-> 2028000.ssi mapping ok
(190605_10:05:54.401)<3>imx-navi sound1: ASoC: no source widget found for HPOUTL
(190605_10:05:54.401)<3>imx-navi sound1: ASoC: Failed to add route HPOUTL -> direct -> Headphone Jack
(190605_10:05:54.401)<4>imx_navi_late_probe
(190605_10:05:54.401)<3>navi 2-002a: Unable to sync registers 0x0-0x0. -5
(190605_10:05:54.401)<6>NET: Registered protocol family 26
(190605_10:05:54.401)<6>u32 classifier
(190605_10:05:54.401)<6> Actions configured
(190605_10:05:54.401)<6>Netfilter messages via NETLINK v0.30.
(190605_10:05:54.401)<6>nf_conntrack version 0.5.0 (11552 buckets, 46208 max)
(190605_10:05:54.401)<6>ctnetlink v0.93: registering with nfnetlink.
(190605_10:05:54.401)<6>xt_time: kernel timezone is -0000
(190605_10:05:54.401)<6>ip_tables: (C) 2000-2006 Netfilter Core Team
(190605_10:05:54.401)<6>arp_tables: (C) 2002 David S. Miller
(190605_10:05:54.401)<6>Initializing XFRM netlink socket
(190605_10:05:54.401)<6>NET: Registered protocol family 10
(190605_10:05:54.402)<6>mip6: Mobile IPv6
(190605_10:05:54.402)<6>ip6_tables: (C) 2000-2006 Netfilter Core Team
(190605_10:05:54.402)<6>sit: IPv6 over IPv4 tunneling driver
(190605_10:05:54.402)<6>NET: Registered protocol family 17
(190605_10:05:54.402)<6>NET: Registered protocol family 15
(190605_10:05:54.402)<6>8021q: 802.1Q VLAN Support v1.8
(190605_10:05:54.402)<6>snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
(190605_10:05:54.402)<6>wlreg_on: disabling
(190605_10:05:54.402)<6>ALSA device list:
(190605_10:05:54.402)<6> #0: cs42l52-audio
(190605_10:05:54.402)<6> #1: navi-audio
(190605_10:05:54.402)<6>Freeing unused kernel memory: 1024K (c0b00000 - c0c00000)
(190605_10:05:54.402)<13>init: init started!
(190605_10:05:54.402)<13>init: init second stage started!
(190605_10:05:54.402)<11>init: waitpid failed: No child processes
(190605_10:05:54.402)<11>init: property_set("ro.zygote", "zygote32") failed
(190605_10:05:54.402)<13>init: (Loading properties from /default.prop took 0.00s.)
(190605_10:05:54.402)<13>init: (Parsing /init.environ.rc took 0.00s.)
(190605_10:05:54.402)<13>init: (Parsing /init.usb.rc took 0.00s.)
(190605_10:05:54.402)<11>init: /init.freescale.rc: 164: invalid option 'mkdir'
(190605_10:05:54.402)<11>init: /init.freescale.rc: 165: invalid option 'chmod'
(190605_10:05:54.402)<11>init: /init.freescale.rc: 166: invalid option 'chmod'
(190605_10:05:54.402)<11>init: /init.freescale.rc: 167: invalid option 'chown'
(190605_10:05:54.402)<11>init: /init.freescale.rc: 168: invalid option 'chown'
(190605_10:05:54.402)<11>init: /init.freescale.rc: 171: invalid option 'mkdir'
(190605_10:05:54.460)<11>init: /init.freescale.rc: 172: invalid option 'mkdir'
(190605_10:05:54.462)<11>init: /init.freescale.rc: 173: invalid option 'chmod'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 174: invalid option 'chmod'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 175: invalid option 'chown'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 176: invalid option 'chown'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 178: invalid option 'mkdir'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 180: invalid option 'mkdir'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 181: invalid option 'chmod'
(190605_10:05:54.463)<11>init: /init.freescale.rc: 184: invalid option 'chmod'
(190605_10:05:54.463)<13>init: (Parsing init.freescale.usb.rc took 0.00s.)
(190605_10:05:54.463)<13>init: (Parsing init.freescale.i.MX6Q.rc took 0.00s.)
(190605_10:05:54.463)<13>init: (Parsing /init.freescale.rc took 0.00s.)
(190605_10:05:54.463)<13>init: (Parsing /init.usb.configfs.rc took 0.00s.)
(190605_10:05:54.463)<13>init: (Parsing /init.trace.rc took 0.00s.)
(190605_10:05:54.463)<13>init: (Parsing /init.rc took 0.01s.)
(190605_10:05:54.463)<13>init: Starting service 'ueventd'...
(190605_10:05:54.463)<13>init: Waiting for /dev/.coldboot_done...
(190605_10:05:54.463)<13>ueventd: ueventd started!
(190605_10:05:54.463)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.463)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.463)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.463)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.463)<6>usb 1-1: USB disconnect, device number 3
(190605_10:05:54.463)<13>ueventd: Coldboot took 0.11s.
(190605_10:05:54.463)<13>init: Waiting for /dev/.coldboot_done took 0.12s.
(190605_10:05:54.463)<11>init: /dev/hw_random not found
(190605_10:05:54.463)<13>init: (console_init_action console=ttymxc0.)
(190605_10:05:54.463)<13>init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
(190605_10:05:54.463)<13>init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
(190605_10:05:54.463)<13>init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
(190605_10:05:54.463)<13>init: Starting service 'watchdogd'...
(190605_10:05:54.463)<6>Console: switching to colour dummy device 80x30
(190605_10:05:54.463)<11>init: /dev/hw_random not found
(190605_10:05:54.463)<13>watchdogd: watchdogd started (interval 10, margin 20)!
(190605_10:05:54.463)<11>init: uboot version0 = )
(190605_10:05:54.463)<11>init: uboot version1 = Jan 10 2019 - 21:14:50
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p5): mounted filesystem with ordered data mode. Opts: barrier=1
(190605_10:05:54.463)<14>fs_mgr: __mount(source=/dev/block/mmcblk3p5,target=/system,type=ext4)=0
(190605_10:05:54.463)<4>EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option
(190605_10:05:54.463)<6>usb 1-1: new high-speed USB device number 4 using ci_hdrc
(190605_10:05:54.463)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.463)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.463)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.463)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.463)<6>usb 1-1: USB disconnect, device number 4
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p4): recovery complete
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
(190605_10:05:54.463)<14>fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0
(190605_10:05:54.463)<4>EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p6): recovery complete
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
(190605_10:05:54.463)<14>fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)
(190605_10:05:54.463)<14>fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0
(190605_10:05:54.463)<4>EXT4-fs (mmcblk3p10): Ignoring removed nomblk_io_submit option
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p10): recovery complete
(190605_10:05:54.463)<6>EXT4-fs (mmcblk3p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
(190605_10:05:54.463)<14>fs_mgr: __mount(source=/dev/block/mmcblk3p10,target=/skypine,type=ext4)=0
(190605_10:05:54.463)<4>function_make name = ffs.adb
(190605_10:05:54.463)<6>file system registered
(190605_10:05:54.463)<4>function_make name = mtp.gs0
(190605_10:05:54.463)<4>function_make name = ptp.gs1
(190605_10:05:54.463)<4>function_make name = accessory.gs2
(190605_10:05:54.463)<4>function_make name = audio_source.gs3
(190605_10:05:54.463)<4>function_make name = rndis.gs4
(190605_10:05:54.463)<4>function_make name = midi.gs5
(190605_10:05:54.463)<4>function_make name = iap2.gs6
(190605_10:05:54.463)<4>@@@@@@@@@@@@ iap2_alloc_inst
(190605_10:05:54.463)<4>iap2_setup !
(190605_10:05:54.463)<4>function_make name = ncm.gs7
(190605_10:05:54.463)<4>@@@@@@@@@@@@ ncm_alloc_inst
(190605_10:05:54.463)<4>using random self ethernet address
(190605_10:05:54.463)<4>using random host ethernet address
(190605_10:05:54.464)<4>function_make name = uac2.gs8
(190605_10:05:54.464)<4>@@@@ afunc_alloc_inst
(190605_10:05:54.464)<4>function_make name = iap2_ext_acc.gs9
(190605_10:05:54.464)<7>EA_DBG: __iap2_ext_acc_setup
(190605_10:05:54.464)<7>EA_DBG: ## iap2_ext_acc_set_disconnected 0
(190605_10:05:54.464)<13>init: Starting service 'logd'...
(190605_10:05:54.464)<13>init: (Loading properties from /skypine/serialno.txt took 0.00s.)
(190605_10:05:54.464)<13>init: SET ro.serialno to easy link debug number 1221212122220
(190605_10:05:54.464)<13>init: (Loading properties from /system/build.prop took 0.01s.)
(190605_10:05:54.464)<13>init: (Loading properties from /vendor/build.prop took 0.00s.)
(190605_10:05:54.464)<13>init: (Loading properties from /factory/factory.prop took 0.00s.)
(190605_10:05:54.464)<13>init: Starting service 'vold'...
(190605_10:05:54.464)<13>init: Not bootcharting.
(190605_10:05:54.464)<11>init: Failed to reload policy
(190605_10:05:54.464)<13>init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
(190605_10:05:54.464)<6>usb 1-1: new high-speed USB device number 5 using ci_hdrc
(190605_10:05:54.464)<13>init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 113) exited with status 0
(190605_10:05:54.464)<11>init: do_load_persist_props'1'
(190605_10:05:54.464)<5>random: init urandom read with 29 bits of entropy available
(190605_10:05:54.464)<38>logd.auditd: start
(190605_10:05:54.464)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.464)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.464)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.464)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.464)<6>usb 1-1: USB disconnect, device number 5
(190605_10:05:54.464)<13>init: Starting service 'logd-reinit'...
(190605_10:05:54.464)<13>init: (check_recovery_mode2 property_get return 0,gotorecovery =.)
(190605_10:05:54.464)<13>init: Starting service 'free_highmem'...
(190605_10:05:54.464)<13>init: Starting service 'healthd'...
(190605_10:05:54.464)<13>init: Starting service 'console'...
(190605_10:05:54.464)<13>init: Starting service 'lmkd'...
(190605_10:05:54.464)<13>init: Starting service 'servicemanager'...
(190605_10:05:54.464)<13>init: Starting service 'surfaceflinger'...
(190605_10:05:54.524)<6>binder: 122:122 transaction failed 29189, size 0-0
(190605_10:05:54.527)<13>init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No such file or directory
(190605_10:05:54.527)<13>init: write_file: Unable to open '/sys/block/mmcblk1/queue/read_ahead_kb': No such file or directory
(190605_10:05:54.527)<13>init: write_file: Unable to open '/sys/class/rfkill/rfkill0/state': No such file or directory
(190605_10:05:54.527)<30>logd.daemon: reinit
(190605_10:05:54.527)<13>init: Service 'logd-reinit' (pid 120) exited with status 0
(190605_10:05:54.527)<11>init: property_set("ro.ril.wake_lock_timeout", "300") failed
(190605_10:05:54.527)<13>init: Starting service 'randomMac'...
(190605_10:05:54.527)<13>init: Starting service 'zygote'...
(190605_10:05:54.527)<13>init: Starting service 'netd'...
(190605_10:05:54.527)<13>init: Starting service 'debuggerd'...
(190605_10:05:54.527)<13>init: Starting service 'media'...
(190605_10:05:54.528)<13>init: Starting service 'installd'...
(190605_10:05:54.528)<11>init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'
(190605_10:05:54.528)<13>init: Starting service 'keystore'...
(190605_10:05:54.528)<13>init: Starting service 'mdnsd'...
(190605_10:05:54.528)<13>init: Starting service 'usb_demo'...
(190605_10:05:54.528)<13>init: Starting service 'check_usb_mode'...
(190605_10:05:54.528)<13>init: Starting service 'copy_skp_files'...
(190605_10:05:54.528)<13>init: Starting service 'touchsrceen'...
(190605_10:05:54.528)<13>init: Starting service 'ril-daemon'...
(190605_10:05:54.528)<13>init: Starting service 'brlinkd'...
(190605_10:05:54.528)<11>init: cannot find '/system/xbin/perfprofd', disabling 'perfprofd'
(190605_10:05:54.528)<11>init: cannot find '/system/bin/magd', disabling 'magd'
(190605_10:05:54.528)<13>init: Starting service 'adbd'...
(190605_10:05:54.528)<7>Buffer from user space:
(190605_10:05:54.528)<7>: 03 00 00 00 69 00 00 00 07 00 00 00 03 00 00 00 ....i...........
(190605_10:05:54.528)<7>: 03 00 00 00 05 00 00 00 09 04 00 00 02 ff 42 01 ..............B.
(190605_10:05:54.528)<7>: 01 07 05 01 02 40 00 00 07 05 82 02 40 00 00 09 .....@......@...
(190605_10:05:54.528)<7>: 04 00 00 02 ff 42 01 01 07 05 01 02 00 02 00 07 .....B..........
(190605_10:05:54.528)<7>: 05 82 02 00 02 00 09 04 00 00 02 ff 42 01 01 07 ............B...
(190605_10:05:54.528)<7>: 05 01 02 00 04 00 06 30 00 00 00 00 07 05 82 02 .......0........
(190605_10:05:54.528)<7>: 00 04 00 06 30 00 00 00 00 ....0....
(190605_10:05:54.528)<6>read descriptors
(190605_10:05:54.528)<7>interface descriptor
(190605_10:05:54.528)<7>entity INTERFACE(00)
(190605_10:05:54.528)<7>entity STRING(01)
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(01)
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(82)
(190605_10:05:54.528)<7>interface descriptor
(190605_10:05:54.528)<7>entity INTERFACE(00)
(190605_10:05:54.528)<7>entity STRING(01)
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(01)
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(82)
(190605_10:05:54.528)<7>interface descriptor
(190605_10:05:54.528)<7>entity INTERFACE(00)
(190605_10:05:54.528)<7>entity STRING(01)
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(01)
(190605_10:05:54.528)<7>EP SS companion descriptor
(190605_10:05:54.528)<7>endpoint descriptor
(190605_10:05:54.528)<7>entity ENDPOINT(82)
(190605_10:05:54.528)<7>EP SS companion descriptor
(190605_10:05:54.528)<7>Buffer from user space:
(190605_10:05:54.529)<7>: 02 00 00 00 20 00 00 00 01 00 00 00 01 00 00 00 .... ...........
(190605_10:05:54.529)<7>: 09 04 41 44 42 20 49 6e 74 65 72 66 61 63 65 00 ..ADB Interface.
(190605_10:05:54.529)<6>read strings
(190605_10:05:54.529)<7>udc ci_hdrc.0: registering UDC driver [g1]
(190605_10:05:54.529)<4>@@@@@@@ configfs_composite_bind gadget = 0xd2038318 gadget_info =0xd2ae5800
(190605_10:05:54.529)<7>configfs-gadget gadget: adding 'mtp'/d2896800 to config 'b'/d2896698
(190605_10:05:54.529)<7>configfs-gadget gadget: mtp_function_bind dev: d2896800
(190605_10:05:54.529)<7>configfs-gadget gadget: create_bulk_endpoints dev: d2896800
(190605_10:05:54.529)<7>configfs-gadget gadget: usb_ep_autoconfig for ep_in got ep1in
(190605_10:05:54.529)<7>configfs-gadget gadget: usb_ep_autoconfig for mtp ep_out got ep1out
(190605_10:05:54.529)<7>configfs-gadget gadget: usb_ep_autoconfig for mtp ep_intr got ep2in
(190605_10:05:54.529)<7>configfs-gadget gadget: dual speed mtp: IN/ep1in, OUT/ep1out
(190605_10:05:54.529)<7>configfs-gadget gadget: adding 'Function FS Gadget'/d2ac7564 to config 'b'/d2896698
(190605_10:05:54.529)<7>interface descriptor
(190605_10:05:54.529)<7>entity INTERFACE(00)
(190605_10:05:54.529)<7>entity STRING(01)
(190605_10:05:54.529)<7>: Original ep desc: 07 05 01 02 40 00 00 ....@..
(190605_10:05:54.529)<7>autoconfig
(190605_10:05:54.529)<7>: Rewritten ep desc: 07 05 02 02 40 00 00 ....@..
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(02)
(190605_10:05:54.529)<7>: Original ep desc: 07 05 82 02 40 00 00 ....@..
(190605_10:05:54.529)<7>autoconfig
(190605_10:05:54.529)<7>: Rewritten ep desc: 07 05 83 02 40 00 00 ....@..
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(83)
(190605_10:05:54.529)<7>interface descriptor
(190605_10:05:54.529)<7>entity INTERFACE(00)
(190605_10:05:54.529)<7>entity STRING(01)
(190605_10:05:54.529)<7>: Original ep desc: 07 05 01 02 00 02 00 .......
(190605_10:05:54.529)<7>: Rewritten ep desc: 07 05 02 02 00 02 00 .......
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(02)
(190605_10:05:54.529)<7>: Original ep desc: 07 05 82 02 00 02 00 .......
(190605_10:05:54.529)<7>: Rewritten ep desc: 07 05 83 02 00 02 00 .......
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(83)
(190605_10:05:54.529)<7>interface descriptor
(190605_10:05:54.529)<7>entity INTERFACE(00)
(190605_10:05:54.529)<7>00 -> 01
(190605_10:05:54.529)<7>entity STRING(01)
(190605_10:05:54.529)<7>01 -> 06
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(02)
(190605_10:05:54.529)<7>endpoint descriptor
(190605_10:05:54.529)<7>entity ENDPOINT(83)
(190605_10:05:54.529)<7>interface descriptor
(190605_10:05:54.529)<7>entity INTERFACE(00)
(190605_10:05:54.529)<7>00 -> 01
(190605_10:05:54.530)<7>entity STRING(01)
(190605_10:05:54.530)<7>01 -> 06
(190605_10:05:54.530)<7>endpoint descriptor
(190605_10:05:54.530)<7>entity ENDPOINT(02)
(190605_10:05:54.530)<7>endpoint descriptor
(190605_10:05:54.530)<7>entity ENDPOINT(83)
(190605_10:05:54.530)<7>adding event 0
(190605_10:05:54.530)<13>init: Service 'randomMac' (pid 128) exited with status 0
(190605_10:05:54.530)<4>1-0020 supply avdd not found, using dummy regulator
(190605_10:05:54.530)<4>1-0020 supply vdd not found, using dummy regulator
(190605_10:05:54.530)<6>usb 1-1: new high-speed USB device number 6 using ci_hdrc
(190605_10:05:54.530)<13>init: Starting service 'set_usb_host'...
(190605_10:05:54.530)<13>init: Service 'check_usb_mode' (pid 137) exited with status 0
(190605_10:05:54.530)<4>ci_role_write ci =0xd2038010
(190605_10:05:54.530)<13>init: write_file: Unable to write to '/sys/kernel/debug/ci_hdrc.0/role': Invalid argument
(190605_10:05:54.530)<7>configfs-gadget ci_hdrc.0: unregistering UDC driver [g1]
(190605_10:05:54.530)<3>configfs-gadget gadget: unbind function 'mtp'/d2896800
(190605_10:05:54.530)<3>configfs-gadget gadget: unbind function 'Function FS Gadget'/d2ac7564
(190605_10:05:54.530)<7>purging event 0
(190605_10:05:54.530)<7>adding event 1
(190605_10:05:54.530)<6>acc_alloc
(190605_10:05:54.530)<4>afunc_alloc
(190605_10:05:54.530)<7>udc ci_hdrc.0: registering UDC driver [g1]
(190605_10:05:54.530)<4>@@@@@@@ configfs_composite_bind gadget = 0xd2038318 gadget_info =0xd2ae5800
(190605_10:05:54.530)<7>configfs-gadget gadget: adding 'iap2'/d29989c0 to config 'b'/d2896698
(190605_10:05:54.530)<3>configfs-gadget gadget: create_bulk_endpoints dev: d29989c0
(190605_10:05:54.530)<7>configfs-gadget gadget: usb_ep_autoconfig for ep_in got ep1in
(190605_10:05:54.587)<7>configfs-gadget gadget: usb_ep_autoconfig for iap2 ep_out got ep1out
(190605_10:05:54.590)<6>configfs-gadget gadget: dual speed iap2: IN/ep1in, OUT/ep1out
(190605_10:05:54.590)<7>configfs-gadget gadget: adding 'uac2'/d2a5c010 to config 'b'/d2896698
(190605_10:05:54.590)<4>@@@@ afunc_bind
(190605_10:05:54.590)<6>android_work: sent uevent IPOD_STATE=DISCONNECTED
(190605_10:05:54.590)<4>ci_role_write ci =0xd2038010
(190605_10:05:54.590)<6>ci_hdrc ci_hdrc.0: EHCI Host Controller
(190605_10:05:54.590)<6>ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2
(190605_10:05:54.590)<6>ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
(190605_10:05:54.590)<6>usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
(190605_10:05:54.590)<6>usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
(190605_10:05:54.590)<6>usb usb2: Product: EHCI Host Controller
(190605_10:05:54.590)<6>usb usb2: Manufacturer: Linux 4.1.15-g2a34798-dirty ehci_hcd
(190605_10:05:54.590)<6>usb usb2: SerialNumber: ci_hdrc.0
(190605_10:05:54.590)<6>hub 2-0:1.0: USB hub found
(190605_10:05:54.590)<6>hub 2-0:1.0: 1 port detected
(190605_10:05:54.590)<13>init: Service 'copy_skp_files' (pid 138) exited with status 0
(190605_10:05:54.590)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.590)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.590)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.590)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.590)<6>usb 1-1: USB disconnect, device number 6
(190605_10:05:54.590)<4>@@@@@@free highmem done
(190605_10:05:54.590)<13>init: Service 'free_highmem' (pid 121) exited with status 0
(190605_10:05:54.590)<13>init: Service 'set_usb_host' (pid 160) exited with status 0
(190605_10:05:54.590)<6>usb 1-1: new high-speed USB device number 7 using ci_hdrc
(190605_10:05:54.590)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.590)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.590)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.590)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.590)<6>usb 1-1: USB disconnect, device number 7
(190605_10:05:54.590)<6>input: synaptics_dsx as /devices/soc0/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0020/input/input0
(190605_10:05:54.590)<13>init: Service 'touchsrceen' (pid 139) exited with status 0
(190605_10:05:54.590)<11>healthd: No charger supplies found
(190605_10:05:54.590)<12>healthd: No battery devices found
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.590)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<4>mxc_free_frame_buf cam->frame[i].vaddress = 0x0
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 8 using ci_hdrc
(190605_10:05:54.591)<13>init: Starting service 'bootanim'...
(190605_10:05:54.591)<3>synaptics_dsx_i2c 1-0020: synaptics_rmi4_irq_enable: Interrupt already enabled
(190605_10:05:54.591)<3>usb 1-1: device descriptor read/all, error -71
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 9 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<3>hub 1-1:1.0: config failed, can't get hub status (err -32)
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 9
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 10 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 10
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 11 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 11
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 12 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 12
(190605_10:05:54.591)<6>capability: warning: `Thread-6' uses 32-bit capabilities (legacy support in use)
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 13 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 13
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 14 using ci_hdrc
(190605_10:05:54.591)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.591)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.591)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.591)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.591)<6>usb 1-1: USB disconnect, device number 14
(190605_10:05:54.591)<6>usb 1-1: new high-speed USB device number 15 using ci_hdrc
(190605_10:05:54.648)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.650)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.650)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.650)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.650)<6>usb 1-1: USB disconnect, device number 15
(190605_10:05:54.650)<6>usb 1-1: new high-speed USB device number 16 using ci_hdrc
(190605_10:05:54.650)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.650)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.651)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.651)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.651)<6>usb 1-1: USB disconnect, device number 16
(190605_10:05:54.651)<6>usb 1-1: new high-speed USB device number 17 using ci_hdrc
(190605_10:05:54.837)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:54.840)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:54.840)<6>hub 1-1:1.0: USB hub found
(190605_10:05:54.840)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:54.840)<6>usb 1-1: USB disconnect, device number 17
(190605_10:05:54.960)<4>zram: 412 (system_server) Attribute mem_used_total (and others) will be removed. See zram documentation.
(190605_10:05:55.022)<5>random: nonblocking pool is initialized
(190605_10:05:55.085)<6>usb 1-1: new high-speed USB device number 18 using ci_hdrc
(190605_10:05:55.274)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:55.275)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:55.275)<6>hub 1-1:1.0: USB hub found
(190605_10:05:55.275)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:55.275)<6>usb 1-1: USB disconnect, device number 18
(190605_10:05:55.521)<6>usb 1-1: new high-speed USB device number 19 using ci_hdrc
(190605_10:05:55.711)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:55.712)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:55.712)<6>hub 1-1:1.0: USB hub found
(190605_10:05:55.712)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:55.712)<6>usb 1-1: USB disconnect, device number 19
(190605_10:05:55.958)<6>usb 1-1: new high-speed USB device number 20 using ci_hdrc
(190605_10:05:56.145)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:56.146)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:56.146)<6>hub 1-1:1.0: USB hub found
(190605_10:05:56.146)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:56.146)<6>usb 1-1: USB disconnect, device number 20
(190605_10:05:56.396)<6>usb 1-1: new high-speed USB device number 21 using ci_hdrc
(190605_10:05:56.584)<3>usb 1-1: device descriptor read/all, error -71
(190605_10:05:56.708)<6>usb 1-1: new high-speed USB device number 22 using ci_hdrc
(190605_10:05:56.833)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:56.834)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:56.834)<6>hub 1-1:1.0: USB hub found
(190605_10:05:56.834)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:56.834)<6>usb 1-1: USB disconnect, device number 22
(190605_10:05:57.144)<6>usb 1-1: new high-speed USB device number 23 using ci_hdrc
(190605_10:05:57.270)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:57.271)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:57.271)<6>hub 1-1:1.0: USB hub found
(190605_10:05:57.271)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:57.271)<6>usb 1-1: USB disconnect, device number 23
(190605_10:05:57.581)<6>usb 1-1: new high-speed USB device number 24 using ci_hdrc
(190605_10:05:57.705)<6>usb 1-1: New USB device found, idVendor=0424, idPr
(190605_10:05:57.768)oduct=2514
(190605_10:05:57.769)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:57.769)<6>hub 1-1:1.0: USB hub found
(190605_10:05:57.769)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:57.769)<6>usb 1-1: USB disconnect, device number 24
(190605_10:05:58.019)<6>usb 1-1: new high-speed USB device number 25 using ci_hdrc
(190605_10:05:58.081)<6>lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:
(190605_10:05:58.081)<6>lowmemorykiller: oom_adj 0 => oom_score_adj 0
(190605_10:05:58.082)<6>lowmemorykiller: oom_adj 1 => oom_score_adj 58
(190605_10:05:58.082)<6>lowmemorykiller: oom_adj 2 => oom_score_adj 117
(190605_10:05:58.082)<6>lowmemorykiller: oom_adj 3 => oom_score_adj 176
(190605_10:05:58.082)<6>lowmemorykiller: oom_adj 9 => oom_score_adj 529
(190605_10:05:58.082)<6>lowmemorykiller: oom_adj 15 => oom_score_adj 1000
(190605_10:05:58.144)<
(190605_10:05:58.206)6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:58.207)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:58.207)<6>hub 1-1:1.0: USB hub found
(190605_10:05:58.207)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:58.207)<6>usb 1-1: USB disconnect, device number 25
(190605_10:05:58.454)<6>usb 1-1: new high-speed USB device number 26 using ci_hdrc
(190605_10:05:58.643)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:58.644)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:58.644)<6>hub 1-1:1.0: USB hub found
(190605_10:05:58.644)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:58.644)<6>usb 1-1: USB disconnect, device number 26
(190605_10:05:58.706)<6>acc_open
(190605_10:05:58.707)<6>acc_release
(190605_10:05:58.891)<6>usb 1-1: new high-speed USB device number 27 using ci_hdrc
(190605_10:05:59.078)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:59.079)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:59.079)<6>hub 1-1:1.0: USB hub found
(190605_10:05:59.079)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:59.079)<6>usb 1-1: USB disconnect, device number 27
(190605_10:05:59.328)<6>usb 1-1: new high-speed USB device number 28 using ci_hdrc
(190605_10:05:59.517)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:59.518)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:59.518)<6>hub 1-1:1.0: USB hub found
(190605_10:05:59.518)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:59.518)<6>usb 1-1: USB disconnect, device number 28
(190605_10:05:59.766)<6>usb 1-1: new high-speed USB device number 29 using ci_hdrc
(190605_10:05:59.952)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:05:59.953)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:05:59.953)<6>hub 1-1:1.0: USB hub found
(190605_10:05:59.953)<6>hub 1-1:1.0: 4 ports detected
(190605_10:05:59.953)<6>usb 1-1: USB disconnect, device number 29
(190605_10:06:00.201)<4>request gpio 94
(190605_10:06:00.202)<6>usb 1-1: new high-speed USB device number 30 using ci_hdrc
(190605_10:06:00.265)<4>request gpio 87
(190605_10:06:00.266)<4>gpio 87 already requested!
(190605_10:06:00.266)<4>request gpio 95
(190605_10:06:00.390)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:00.391)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:00.391)<6>hub 1-1:1.0: USB hub found
(190605_10:06:00.391)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:00.391)<6>usb 1-1: USB disconnect, device number 30
(190605_10:06:00.639)<6>usb 1-1: new high-speed USB device number 31 using ci_hdrc
(190605_10:06:00.826)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:00.827)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:00.827)<6>hub 1-1:1.0: USB hub found
(190605_10:06:00.827)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:00.827)<6>usb 1-1: USB disconnect, device number 31
(190605_10:06:01.075)<6>usb 1-1: new high-speed USB devi
(190605_10:06:01.138)ce number 32 using ci_hdrc
(190605_10:06:01.139)<4>request gpio 132
(190605_10:06:01.139)<4>gpio 132 already requested!
(190605_10:06:01.263)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:01.264)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:01.264)<6>hub 1-1:1.0: USB hub found
(190605_10:06:01.264)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:01.264)<6>usb 1-1: USB disconnect, device number 32
(190605_10:06:01.513)<13>init: Service 'bootanim' (pid 209) exited with status 0
(190605_10:06:01.574)<6>usb 1-1: new high-speed USB device number 33 using ci_hdrc
(190605_10:06:01.700)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:01.701)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:01.701)<6>hub 1-1:1.0: USB hub found
(190605_10:06:01.701)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:01.701)<6>usb 1-1: USB disconnect, device number 33
(190605_10:06:02.011)<6>usb 1-1: new high-speed USB device number 34 using ci_hdrc
(190605_10:06:02.075)<4>!!!!! android_comple no reverse
(190605_10:06:02.136)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:02.137)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:02.137)<6>hub 1-1:1.0: USB hub found
(190605_10:06:02.137)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:02.137)<6>usb 1-1: USB disconnect, device number 34
(190605_10:06:02.448)<6>usb 1-1: new high-speed USB device number 35 using ci_hdrc
(190605_10:06:02.573)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:02.574)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:02.574)<6>hub 1-1:1.0: USB hub found
(190605_10:06:02.574)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:02.574)<6>usb 1-1: USB disconnect, device number 35
(190605_10:06:02.885)<6>usb 1-1: new high-speed USB device number 36 using ci_hdrc
(190605_10:06:02.886)<13>init: write_file: Unable to write to '/sys/devices/system/cpu/cpu0/cpufreq/scaling_governor': Invalid argument
(190605_10:06:02.886)<13>init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/timer_rate': No such file or directory
(190605_10:06:02.886)<13>init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/min_sample_time': No such file or directory
(190605_10:06:02.886)<13>init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/go_hispeed_load': No such file or directory
(190605_10:06:03.011)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:03.012)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:03.012)<6>hub 1-1:1.0: USB hub found
(190605_10:06:03.012)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:03.012)<6>usb 1-1: USB disconnect, device number 36
(190605_10:06:03.321)<6>usb 1-1: new high-speed USB device number 37 using ci_hdrc
(190605_10:06:03.446)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:03.447)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:03.447)<6>hub 1-1:1.0: USB hub found
(190605_10:06:03.447)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:03.447)<6>usb 1-1: USB disconnect, device number 37
(190605_10:06:03.758)<6>usb 1-1: new high-speed USB device number 38 using ci_hdrc
(190605_10:06:03.883)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:03.884)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:03.884)<6>hub 1-1:1.0: USB hub found
(190605_10:06:03.884)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:03.884)<6>usb 1-1: USB disconnect, device number 38
(190605_10:06:04.195)<6>usb 1-1: new high-speed USB device number 39 using ci_hdrc
(190605_10:06:04.319)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:04.320)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:04.320)<6>hub 1-1:1.0: USB hub found
(190605_10:06:04.320)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:04.320)<6>usb 1-1: USB disconnect, device number 39
(190605_10:06:04.633)<6>usb 1-1: new high-speed USB device number 40 using ci_hdrc
(190605_10:06:04.759)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:04.760)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:04.760)<6>hub 1-1:1.0: USB hub found
(190605_10:06:04.760)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:04.760)<6>usb 1-1: USB disconnect, device number 40
(190605_10:06:05.068)<6>usb 1-1: new high-speed USB device number 41 using ci_hdrc
(190605_10:06:05.255)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:05.256)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:05.256)<6>hub 1-1:1.0: USB hub found
(190605_10:06:05.256)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:05.256)<6>usb 1-1: USB disconnect, device number 41
(190605_10:06:05.505)<6>usb 1-1: new high-speed USB device number 42 using ci_hdrc
(190605_10:06:05.693)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:05.694)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:05.694)<6>hub 1-1:1.0: USB hub found
(190605_10:06:05.694)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:05.694)<6>usb 1-1: USB disconnect, device number 42
(190605_10:06:05.969)<6>usb 1-1: new high-speed USB device number 43 using ci_hdrc
(190605_10:06:06.145)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:06.146)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:06.146)<6>hub 1-1:1.0: USB hub found
(190605_10:06:06.146)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:06.146)<6>usb 1-1: USB disconnect, device number 43
(190605_10:06:06.397)<6>usb 1-1: new high-speed USB device number 44 using ci_hdrc
(190605_10:06:06.581)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:06.582)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:06.582)<6>hub 1-1:1.0: USB hub found
(190605_10:06:06.582)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:06.582)<6>usb 1-1: USB disconnect, device number 44
(190605_10:06:06.831)<6>usb 1-1: new high-speed USB device number 45 using ci_hdrc
(190605_10:06:07.019)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:07.020)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:07.020)<6>hub 1-1:1.0: USB hub found
(190605_10:06:07.020)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:07.020)<6>usb 1-1: USB disconnect, device number 45
(190605_10:06:07.268)<6>usb 1-1: new high-speed USB device number 46 using ci_hdrc
(190605_10:06:07.455)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:07.456)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:07.456)<6>hub 1-1:1.0: USB hub found
(190605_10:06:07.456)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:07.456)<6>usb 1-1: USB disconnect, device number 46
(190605_10:06:07.705)<6>usb 1-1: new high-speed USB device number 47 using ci_hdrc
(190605_10:06:07.894)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:07.894)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:07.895)<6>hub 1-1:1.0: USB hub found
(190605_10:06:07.895)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:07.895)<6>usb 1-1: USB disconnect, device number 47
(190605_10:06:08.206)<6>usb 1-1: new high-speed USB device number 48 using ci_hdrc
(190605_10:06:08.330)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:08.331)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:08.331)<6>hub 1-1:1.0: USB hub found
(190605_10:06:08.331)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:08.331)<3>hub 1-1:1.0: config failed, can't get hub status (err -32)
(190605_10:06:08.331)<6>usb 1-1: USB disconnect, device number 48
(190605_10:06:08.640)<6>usb 1-1: new high-speed USB device number 49 using ci_hdrc
(190605_10:06:08.829)<3>usb 1-1: device descriptor read/all, error -71
(190605_10:06:08.952)<6>usb 1-1: new high-speed USB device number 50 using ci_hdrc
(190605_10:06:09.077)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:09.078)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:09.078)<6>hub 1-1:1.0: USB hub found
(190605_10:06:09.078)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:09.078)<6>usb 1-1: USB disconnect, device number 50
(190605_10:06:09.391)<6>usb 1-1: new high-speed USB device number 51 using ci_hdrc
(190605_10:06:09.516)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:09.517)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:09.517)<6>hub 1-1:1.0: USB hub found
(190605_10:06:09.517)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:09.517)<6>usb 1-1: USB disconnect, device number 51
(190605_10:06:09.826)<6>usb 1-1: new high-speed USB device number 52 using ci_hdrc
(190605_10:06:09.953)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:09.954)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:09.954)<6>hub 1-1:1.0: USB hub found
(190605_10:06:09.954)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:09.954)<6>usb 1-1: USB disconnect, device number 52
(190605_10:06:10.263)<6>usb 1-1: new high-speed USB device number 53 using ci_hdrc
(190605_10:06:10.389)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:10.390)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:10.390)<6>hub 1-1:1.0: USB hub found
(190605_10:06:10.390)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:10.390)<6>usb 1-1: USB disconnect, device number 53
(190605_10:06:10.701)<6>usb 1-1: new high-speed USB device number 54 using ci_hdrc
(190605_10:06:10.825)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:10.826)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:10.826)<6>hub 1-1:1.0: USB hub found
(190605_10:06:10.826)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:10.826)<6>usb 1-1: USB disconnect, device number 54
(190605_10:06:11.138)<6>usb 1-1: new high-speed USB device number 55 using ci_hdrc
(190605_10:06:11.264)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:11.266)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:11.266)<6>hub 1-1:1.0: USB hub found
(190605_10:06:11.266)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:11.266)<6>usb 1-1: USB disconnect, device number 55
(190605_10:06:11.573)<6>usb 1-1: new high-speed USB device number 56 using ci_hdrc
(190605_10:06:11.699)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:11.702)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:11.702)<6>hub 1-1:1.0: USB hub found
(190605_10:06:11.702)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:11.702)<6>usb 1-1: USB disconnect, device number 56
(190605_10:06:12.011)<6>usb 1-1: new high-speed USB device number 57 using ci_hdrc
(190605_10:06:12.137)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:12.137)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:12.137)<6>hub 1-1:1.0: USB hub found
(190605_10:06:12.137)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:12.137)<6>usb 1-1: USB disconnect, device number 57
(190605_10:06:12.449)<6>usb 1-1: new high-speed USB device number 58 using ci_hdrc
(190605_10:06:12.573)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:12.575)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:12.575)<6>hub 1-1:1.0: USB hub found
(190605_10:06:12.575)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:12.575)<6>usb 1-1: USB disconnect, device number 58
(190605_10:06:12.886)<6>usb 1-1: new high-speed USB device number 59 using ci_hdrc
(190605_10:06:13.009)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:13.010)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:13.010)<6>hub 1-1:1.0: USB hub found
(190605_10:06:13.010)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:13.010)<6>usb 1-1: USB disconnect, device number 59
(190605_10:06:13.321)<6>usb 1-1: new high-speed USB device number 60 using ci_hdrc
(190605_10:06:13.448)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:13.448)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:13.448)<6>hub 1-1:1.0: USB hub found
(190605_10:06:13.448)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:13.448)<6>usb 1-1: USB disconnect, device number 60
(190605_10:06:13.760)<6>usb 1-1: new high-speed USB device number 61 using ci_hdrc
(190605_10:06:13.885)<6>
(190605_10:06:13.947)usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:13.949)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:13.949)<6>hub 1-1:1.0: USB hub found
(190605_10:06:13.949)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:13.949)<6>usb 1-1: USB disconnect, device number 61
(190605_10:06:14.195)<6>usb 1-1: new high-speed USB device number 62 using ci_hdrc
(190605_10:06:14.382)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:14.384)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:14.384)<6>hub 1-1:1.0: USB hub found
(190605_10:06:14.384)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:14.384)<6>usb 1-1: USB disconnect, device number 62
(190605_10:06:14.631)<6>usb 1-1: new high-speed USB device number 63 using ci_hdrc
(190605_10:06:14.819)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:14.819)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:14.819)<6>hub 1-1:1.0: USB hub found
(190605_10:06:14.819)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:14.819)<6>usb 1-1: USB disconnect, device number 63
(190605_10:06:15.068)<6>usb 1-1: new high-speed USB device number 64 using ci_hdrc
(190605_10:06:15.257)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:15.257)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:15.258)<6>hub 1-1:1.0: USB hub found
(190605_10:06:15.258)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:15.258)<6>usb 1-1: USB disconnect, device number 64
(190605_10:06:15.507)<6>usb 1-1: new high-speed USB device number 65 using ci_hdrc
(190605_10:06:15.692)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:15.693)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:15.693)<6>hub 1-1:1.0: USB hub found
(190605_10:06:15.693)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:15.693)<6>usb 1-1: USB disconnect, device number 65
(190605_10:06:15.944)<6>usb 1-1: new high-speed USB device number 66 using ci_hdrc
(190605_10:06:16.130)<6>usb 1-1: New USB device found, idVendor=0424, idProduct=2514
(190605_10:06:16.131)<6>usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
(190605_10:06:16.131)<6>hub 1-1:1.0: USB hub found
(190605_10:06:16.131)<6>hub 1-1:1.0: 4 ports detected
(190605_10:06:16.131)<6>usb 1-1: USB disconnect, device number 66
(190605_10:06:16.379)<6>usb 1-1: new high-speed USB device number 67 using ci_hdrc

0 Kudos
Reply

1,843 Views
Yuri
NXP Employee
NXP Employee

Hello,

  perhaps it makes sense to check memory again.

https://community.nxp.com/docs/DOC-105652

Regards,

Yuri.

0 Kudos
Reply