I.MX6Q Nand Flash Interface Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q Nand Flash Interface Problem

2,666 Views
mithunp_s
Contributor III

Dear All,

One of my customer is using MCIMX6QAICPU1, they want Uboot kernal to run on NOR Flash and File system run on NAND. When we use Micron Flash SLC NAND Flash 8Gbits (1GB) MT29F8G08ABABAWP and tested it is able to recognize Nand Flash and Initialize successfully.


But whey we MLC NAND Flash of 32Gbits (4GB)   MT29F32G08CBADA , it is able to recognize nand Flash but while Initializing its getting crash.

Please help to resolve this, please also let us know if this supports 32GB Nand flash.

Regards

Mithun

0 Kudos
Reply
4 Replies

2,357 Views
mithunp_s
Contributor III

Hi All,

We are getting below error

NAND device: Manufacturer ID: 0x2c, Chip ID: 0x44 (Micron MT29F32G08CBADAWP)
gpmi-nand imx6q-gpmi-nand.0: enable asynchronous EDO mode 5
Scanning device for bad blocks
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = 80004000
[00000000] *pgd=00000000
Internal error: Oops: 5 [#1] PREEMPT SMP
Modules linked in:
CPU: 0    Not tainted  (3.0.35-4.1.0+yocto+gbdde708 #1)
PC is at gpmi_send_command+0x5c/0x118


0 Kudos
Reply

2,357 Views
YixingKong
Senior Contributor IV

Mithun

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

2,357 Views
YixingKong
Senior Contributor IV

Mithun

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

2,357 Views
YixingKong
Senior Contributor IV

Mithun

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply