I.MX6Q HDMI Output!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q HDMI Output!

1,816件の閲覧回数
tommyduan
Contributor III
  • We are now designing an HDMI output to connect to the TV,We found that HDMI devices could not be detected by TV if the connection was made with HDMI wires about 5m in length!When I use 2m length, TV can detect it! Is chip drive ability insufficient?Or which software or hardware parameters can be modified?How far can our chip connect to HDMI output?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,699件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tommy

one can look on

How to adjusting HDMI strength 

recheck hdmi layout recommendations given in  i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

sect.4.2.3.2 Reference Cable Equalizer HDMI specification, terminations and measure Eye Diagram

at receiver end.

May be useful AN4671 i.MX 6 Series HDMI Test Method

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,699件の閲覧回数
tommyduan
Contributor III

Thanks fou your reply!

I have a question, after the I.MX6 processor is connected to the TV, how is the HDMI output resolution set?What is the output based on what?

0 件の賞賛
返信