I.MX6Q HDMI Output!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q HDMI Output!

636 Views
tommyduan
Contributor III
  • We are now designing an HDMI output to connect to the TV,We found that HDMI devices could not be detected by TV if the connection was made with HDMI wires about 5m in length!When I use 2m length, TV can detect it! Is chip drive ability insufficient?Or which software or hardware parameters can be modified?How far can our chip connect to HDMI output?

Labels (2)
0 Kudos
2 Replies

519 Views
igorpadykov
NXP Employee
NXP Employee

Hi tommy

one can look on

How to adjusting HDMI strength 

recheck hdmi layout recommendations given in  i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

sect.4.2.3.2 Reference Cable Equalizer HDMI specification, terminations and measure Eye Diagram

at receiver end.

May be useful AN4671 i.MX 6 Series HDMI Test Method

http://cache.freescale.com/files/32bit/doc/app_note/AN4671.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

519 Views
tommyduan
Contributor III

Thanks fou your reply!

I have a question, after the I.MX6 processor is connected to the TV, how is the HDMI output resolution set?What is the output based on what?

0 Kudos