I.MX6 using HAB key in kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 using HAB key in kernel

1,818件の閲覧回数
zc_tee
Contributor III

Hi all,

Is there any example where i can use the private key that was fused inside the i.mx6 chip (for secure boot) to do some authentication of some files during kernel boot up?

I had managed to fused the key into i.mx6 chip, and managed to authenticate u-boot (from boot ROM) and kernel (from u-boot). However, i have no idea how to continue to use the key in kernel to further authenticate some files in filesystem.

Any help is appreciated.

Thank you.

Regards,

Tee

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,486件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I send the document and application note to you for reference,

if you don't think this is enough,  do you mind creating a ticket, then I sent the mail to you. because this is security part, I'm not sure I can share these information publicly,

<Encrypted U-boot Example >.

<http://cache.nxp.com/files/32bit/doc/app_note/AN4581.pdf?fsrch=1&sr=1&pageNum=1 >.

<How to submit a new question for NXP Support >

0 件の賞賛
返信

1,486件の閲覧回数
zc_tee
Contributor III

Anybody has answer for this?

Regards,

Tee

0 件の賞賛
返信