I.MX6 camera interface hardware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 camera interface hardware

3,764件の閲覧回数
erdempamuk
Contributor I

Hi guys

we develop a board with imx6 solo  with camera interface.

1.  Should I use MIPI or parallel interface 

2.  Should I need external components (logic level converters, etc ) to connect imx6 camera sensor interface to cameras like below

  2PCS LOT Phone camera module OV5640+free shipping-in Integrated Circuits from Electronic Components ...

OV5640 low cost 5M pixel long golden finger flex micro camera module 24pin auto focus function-in Ot... 

Af ov5640 automatic webcam module 500 pixels mobile phone webcam module-inOther Electronic Component...

1 返信

1,742件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi erdem

please look at Freescale reference board schematic, it shows connections

for both MIPI and parallel interfaces

i.MX6_SABRE_SDP_DESIGNFILES

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信