I.MX6 android4.4.3-2.0.0 patch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 android4.4.3-2.0.0 patch

5,671 Views
haifengjin
Contributor II

hi  NXP:

             我一直用的是android4.4.3,但是android4.4.3-2.0.0有一个patch,目前官网已经不能下载, android_KK4.4.3_2.0.0-ga_core_source.tar.gz,这个目前能提供吗

Labels (1)
0 Kudos
Reply
6 Replies

5,096 Views
walfredwang
Contributor I

请问你获得这个patch文件了没,能否共享下

0 Kudos
Reply

5,096 Views
haifengjin
Contributor II

链接:http://pan.baidu.com/s/1kV3NNCF 密码:gkc3   网盘上我共享给你

0 Kudos
Reply

5,037 Views
liangyan
Contributor III

hi haifengjin

您好,能给我分享一下吗?

0 Kudos
Reply

5,036 Views
liangyan
Contributor III

感谢,可以下载的。网盘

0 Kudos
Reply

5,096 Views
igorpadykov
NXP Employee
NXP Employee

Hi Haifeng

please create service request so additional help could be provided to you:
https://community.freescale.com/docs/DOC-329745

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,096 Views
haifengjin
Contributor II

OK,非常感谢

0 Kudos
Reply