I.MX6 Android M boot optimization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 Android M boot optimization

2,645 Views
deepika_t
Contributor IV

Hi

I have ported Android M on i.mx6 Sabreauto.

I was going through Android boot optimization - A new try on i.MX6   and http://www.elinux.org/images/d/d1/Alexandre_Belloni_boottime_optimizations.pdf .

We want to optimize Android M so that the Android boots up in 8s.

The Android boot optimization was done on 4.4 Kitkat. Is it possible to do same optimization for Android M.

Also I went through https://community.nxp.com/docs/DOC-93619  . I need to enable MMU and L2 cache in bootloader. Can anyone help me to achieve the same

Thanks

Deepika Teriar

0 Kudos
Reply
3 Replies

2,050 Views
deepika_t
Contributor IV

Hi ,

I want the home screen to come within 10 sec for Android M.

Thanks for sharing the link for MMU and caches

Thanks and regards

Deepika

0 Kudos
Reply

2,050 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Deepika,

Do you need to boot in 8s or inititialize android in 8 secs? document you have suggested show how to boot in 8 secs but initialize in ~25secs.

For MMU and L2Cache please check:

https://community.nxp.com/thread/315745 


Regards

0 Kudos
Reply

2,050 Views
deepika_t
Contributor IV

Hi Folks!!!

Any Suggestions on the questions above?

Thanks

0 Kudos
Reply