I.MX53 wince 7 develop Problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX53 wince 7 develop Problem?

2,612 Views
stevenhsu
Contributor I

Hi~

I am newbie in imx53,BSP is (WEC7 Binary Image by Adeneo).

My question is

1. Can I put some applications in the system (like a vedio-player or image-editor from my laptop) through

    windows mobile center? 

2. Moreover, if I want to run a app (from Windows phone 7, like a game or something) in above wince

   system, what should I do? Do I need to create a UI or something use SDK ?

Please kindly give me a hint or brief description~thanks a lot !

My mailbox: [email protected]

Steven

from Taiwan

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

2,372 Views
iMXAndrew
Contributor II

Steven,

 

If you have the source C++ code you can build a UI and implement in your UI or as a stand alone program. If you implement in a UI you would typically use Silverlight for Embedded and VS2008 with platform builder.

0 Kudos
Reply