I.MX53 and Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX53 and Android

1,526 Views
sileshidemesie
Contributor I

We are using linux on imx.53 qsb these days. Now we want to use android on the same board. For linux we got "MCIMX535-START-R-BSP-11-09_C" image where we use to port ubuntu on SD card. Is there anything in the same way for android also? or Could you please give me a brief explanation on how to port android on SD card so that we can boot android from the SD card.

Thank you so much in advance

Labels (2)
0 Kudos
Reply
1 Reply

1,374 Views
Yuri
NXP Employee
NXP Employee

Please use Android from Adeneo :

http://www.adeneo-embedded.com/Products/Board-Support-Packages/Freescale-i.MX53-QSB

Also the following Community thread may be helpful :

https://community.freescale.com/message/274757#274757


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply