I.MX27 LCD Interfacing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX27 LCD Interfacing

1,544件の閲覧回数
cédricbusinger
Contributor I

Good morning everyone,

I'm using a development kit from armadeus (apf27 development kit) which use the I.MX27 processor. A linux embedded OS (kernel version 2.6.29.6) already run on it. I want to interface the I.MX27 with a LCD (SP14Q006 from Hitachi see link below) using the framebuffer driver.Now here is the problem.

My LCD is a STN monochrome type (1 bit per pixel) and I have heard that the actual framebuffer version doesn't support this type of format.

I want to know if some people already had this type of problem or already have interface this LCD witch the I.MX27 ?

datasheet:

LCD:

http://www.farnell.com/datasheets/3325.pdf

In advance thank you very much for your help

Have a nice day

Regards


Cédric

ラベル(3)
0 件の賞賛
返信
1 返信

1,355件の閲覧回数
Vijayaragavan
Contributor I

Hi

Am also trying for the same with different LCD pixel configration that is 128x64.Any one in the forum please reply or throw some points on this.l Linux Kernel does come with driver support for this kind of interface.

0 件の賞賛
返信