I.MX-qtapplication source code question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX-qtapplication source code question

4,381 Views
kangmw086
Contributor III

hi

my yocto version is morty(kernel 4.9.11)

build-x11.

After booting the x11, it checked the IMX camera application.
I found the image in the following path but not the source code. Can you provide it to source code me?

YOCTO_DIR/build-x11/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/imx-qtapplications/1.2.0-aarch32-r0/

thangs.
regards.

Tags (2)
0 Kudos
Reply
7 Replies

4,353 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think there should have some example code in QT developer forum.

e.g. https://doc.qt.io/archives/qt-5.11/qtmultimedia-index.html

 

For the i.MX, there is imx-test package include the code examples of capture.

0 Kudos
Reply

4,342 Views
kangmw086
Contributor III

sorry, but it's not the software I'm looking for.

The software I want seems to be made by NXP.

In the attached picture below,

I want the source code for the iMX Camera application.

The second picture is the executed screen.

( yocto morty build-x11. kernel 4.9.11 )

a.pnga2.png

 

thank you.

0 Kudos
Reply

4,335 Views
jimmychan
NXP TechSupport
NXP TechSupport

Sorry, we don't provide the source code.

0 Kudos
Reply

4,332 Views
kangmw086
Contributor III

Is there no source code?
Or don't you provide technical support for the source code?

Is it possible to give advice on implementing software such as camera switching, preview, recording, etc.?

For example, using Gstremaer? How to use and handle v4l2?

 

thank you.

0 Kudos
Reply

4,327 Views
jimmychan
NXP TechSupport
NXP TechSupport

We have the imx-test package in Yocto BSP. You can find the source code of V4L2 example there.

 

0 Kudos
Reply

4,320 Views
kangmw086
Contributor III

I checked the V4L2 example (mxc_v4l2_*.out).
I want to know how to make mp4, avi, and jpg in this example.

Can you help me?

regards.

0 Kudos
Reply

4,313 Views
jimmychan
NXP TechSupport
NXP TechSupport

Here is the Linux BSP release web page

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

You can download the documentation for the release version that you are using.

e.g.

The i.MX Linux Reference Manual​ also talk about the V4L2 driver and the unit test.  And the i.MX VPU API Reference Manual​ talk about the VPU API usage.

0 Kudos
Reply