I.MX processor, Yocto Linux, LED state during boot operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX processor, Yocto Linux, LED state during boot operation

1,738 Views
_ZZ_
Contributor II

Hi Everyone,

I have an I.MX custom board running Yocto Linux. The board has two RGB LEDs (in total 6 LEDs), all have been defined in the device tree, accessible from the /sys/class/leds/ and work well in terms of functionality.

my question is that How do I turn on all the LEDs while the board is boot up and reset operation?    some say could be done somewhere in uboot source code though.  

Thanks for any help,

 

0 Kudos
Reply
1 Reply

1,712 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

I suggest you check the next link and take a look on "default-state" LED sub-node properties on device tree. 

Best regards.

Jorge.

0 Kudos
Reply