I.MX Yoco Liux meta-rust layer issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX Yoco Liux meta-rust layer issue

1,819件の閲覧回数
_ZZ_
Contributor II

Hello everyone,

I am experiencing an I.MX yocto build error related to the meta-rust layer which I was not seeing before during the bitebake building process. below it the error line, 

ERROR: Task (virtual:native:/home/dand/yocto/sti_git_repos/firmware_yocto/poky/../meta-rust/recipes-devtools/rust/rust_1.43.0.bb:do_compile) failed with exit code '1'

I wonder if anyone has seen this before and knows the solution

thanks,

0 件の賞賛
返信
2 返答(返信)

1,762件の閲覧回数
_ZZ_
Contributor II

after few times trying, it just went though successfully. not sure what was wrong. It is OK now

1,802件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello!

It make me thing that the Rust version that you are using is not compatible. Please check if the version that you are using is the correct.

 

Best regards!

0 件の賞賛
返信