I. MX 8mn ddr3levk yocto project build problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I. MX 8mn ddr3levk yocto project build problem

1,532 Views
jack_huang1
Contributor IV

Dear:

     I use the ubantu 20.04 virtual machine

     I use the next command to build the imx8mnddr3levk linux L5.10.35.2.0.0

 

$ DISTRO=fsl-imx-xwayland MACHINE=imx8mnddr3levk source imx-setup-release.sh -b imx8mnD3l_l535xwayland

 

$ bitbake imx-image-multimedia

 

At the end of “bitbake imx-image-multimedia”, do-image-wic generate an error, reference this error with the log file “log.do_image_wic.17779”

The log file is attached.

Thank you!

 

 

0 Kudos
Reply
2 Replies

1,510 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello Jack.

For better understand this problem, please provide details as followings:

What steps you have taken before the image build?

what the Virtual machine is and its version? 

Best regards

Harvey

0 Kudos
Reply

1,507 Views
jack_huang1
Contributor IV

After changing the Ubuntu version 18.04, the problem is resolved.Thank you!