I.MX 8 glReadPixels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX 8 glReadPixels

3,121 次查看
holmekj2
Contributor I

We are using a Boundary Devices I.MX8 quad board. We have noticed that when using the Weston screen capture functionality, the display is corrupted (i.e. the windows on the screen are still visible but the pixel color and alignment is scrambled). After several seconds, the screen returns to normal.

After some tracing it looks to happen anytime the glReadPixels call is made in Weston's gl-renderer. Does anyone know a fix or workaround for this behavior.

0 项奖励
回复
3 回复数

2,860 次查看
s_stefanek
Contributor I

I have found this problem too. The device is a Variscite imx8q. I'm trying to make the weston rdp screen-sharing feature work and I also have found that reading the screen contents via glReadPixels() inside the gl-renderer causes screen corruption. The images are still kind-of-recognizable but the colors and the glyphs on the screen are scrambled. Intuitively I'd say that there is some timing issue at the output-to-screen generation stage. The interesting thing is that the output of glReadPixels() is correct: rdp screen-sharing works. It's the local screen output that gets corrupted.
I have also tried the latest kernel module and imx-gpu-viv binary blob (6.4.0.p2). Same result.

Anybody found a solution to this?

0 项奖励
回复

2,860 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Maybe, he can help you.

GaryBisson‌

0 项奖励
回复

2,860 次查看
george
Senior Contributor II

Dear Bio_TICFSL‌,

In our case it is i.MX8M, but we have the same problem.

Is "Gary Bisson" you say is an employee of the boundary device?

Best Regards,

George

0 项奖励
回复