Hybrid Automotive OS(Linux + Android)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hybrid Automotive OS(Linux + Android)

4,703 Views
himabindu
Contributor III

Hi Team,

       I  have generated a yocto  Linux  AGL image for imx8mq evk board. Now how to make common kernel with automotive changes done using yocto such that linux+android  will be supported. Based on some input like android, android has to boot and if input is linux then linux has to boot.

 

Is it possible to make a common kernel(Linux+ Android) with automotive changes for IMX8M evk board.

 

Thanks & Regards,

C.Himabindu.

 

 

 

Labels (1)
0 Kudos
Reply
5 Replies

4,680 Views
himabindu
Contributor III

 

Hi Team,

Can we try the imx8qm-mek images on the imx8mq-evk board .Will the board poweron.

 

Thanks & Regards,

C.Himabindu

0 Kudos
Reply

4,669 Views
art
NXP Employee
NXP Employee

No, it is not possible to run the imx8qm-mek image on the i.MX8MQuad EVK board, since the hardware (including processors) is absolutely incompatible.

Best Regards,

Artur

0 Kudos
Reply

4,680 Views
himabindu
Contributor III

Thankyou for your response

0 Kudos
Reply

4,686 Views
art
NXP Employee
NXP Employee

Q. Is it possible to make a common kernel(Linux+ Android) with automotive changes for IMX8M evk board.

A. Seems that nobody has tried to do it so far.

The Embedded Linux and Android Auto BSPs, supported by NXP, are available separately:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

https://www.nxp.com/design/software/embedded-software/software-technology-for-android-auto:ANDROID-A...

Moreover, only the i.MX8QuadMax SoC is currently supported for Android Auto by NXP.

Best Regards,
Artur

0 Kudos
Reply

3,226 Views
Hassan_Zafirul
Contributor I

I hope someone has done this; could you please provide the links? I'm seeking for this type of solution.

0 Kudos
Reply