How use max9286 in the imx6q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How use max9286 in the imx6q?

1,151 Views
Nian8113
Contributor I

Hi everyone,

  I referenced the max9286 patches.

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

  Then, I can find 4 devices (like /dev/video0, /dev/video1...) in the system.

  But I wish max9286 can combination of 4 cameras to one device (only /dev/video0) in the system.

  Have any idea or suggestion?

  I use L4.1.15_2.0.0-ga BSP.

Thanks.

0 Kudos
Reply
0 Replies