How use kernel driver module for ADV7280-m?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How use kernel driver module for ADV7280-m?

1,849件の閲覧回数
olegoleguello
Contributor II

Hello, I have adv7280-m board and humming board (imx6). I connect  CLKP, CLKN, DOP, DON to MIPI CSI-2.  adv7280- m programed throw windows mashine. How I can use driver module to start capture video from /dev/videoX ?
   $dmesg | grep video
[ 1.588713] mxc_v4l2_output v4l2_out.33: V4L2 device registered as video16
[ 1.588884] mxc_v4l2_output v4l2_out.33: V4L2 device registered as video17
[ 2.615863] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected reports DVI mode
[ 15.678222] V4L2 device 'Mxc Camera' on IPU1_CSI1 registered as video0

 $v4l2-ctl --set-fmt-video=width=1920,height=1088,pixelformat=4
Failed to open /dev/video0: Resource temporarily unavailable

$ ffprobe /dev/video0

Failed to open /dev/video0: Resource temporarily unavailable

root@linux:~# dmesg | grep Camera
[ 15.678222] V4L2 device 'Mxc Camera' on IPU1_CSI1 registered as video0
[ 16.096492] mxc_v4l_open: Mxc Camera no sensor ipu0/csi1
[ 2810.261283] mxc_v4l_open: Mxc Camera no sensor ipu0/csi1

Sorry,  if question is stupid.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,576件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot give support to the humming board. For that I highly recommend you to go to the SolidRun community.

http://forum.solid-run.com/ 

I apologize for this inconvenient.

Best regards,

Diego.

0 件の賞賛
返信