How to verify whether the DDRAM connected to imx6 processor , is in self refresh mode ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to verify whether the DDRAM connected to imx6 processor , is in self refresh mode ?

978 次查看
prakeerthi_y
Contributor I

In free-scale solo board,2 DDR RAMs placed in the board. While optimizing power , we tried to test to put the DDR into self refreshing mode. But I cant create a scenario ,where I can see the self-refresh mode enabled bit in MMDC Control and status register (25 bit) ..Need assistance in how to test the working of self refresh mode..

Thank you.

标签 (4)
0 项奖励
回复
1 回复

906 次查看
igorpadykov
NXP Employee
NXP Employee

Hi prakeerthi

there is no one bit settings and entering self-refresh mode is performed

during procedure described in sect.44.4.6.2 Self refresh and Frequency change

entry/exit i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

One can check with oscilloscope signals described here.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复