How to verify signed image on softhsm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to verify signed image on softhsm

2,750 Views
pawar_123_y
Contributor II

Hello,

I have signed image for AHAB. I want to verify signed image on softhsm to know image is properly signed or not. can you please guide me.

 

Thanks.

0 Kudos
Reply
3 Replies

2,739 Views
b36401
NXP Employee
NXP Employee

Actually HAB API library is included as a component of the boot ROM.
It allows image code, external to the ROM, to make calls back to the HAB for authenticating additional boot stages.
However unfortunately we do not have Linux user space implementation of HAB API.

0 Kudos
Reply

2,733 Views
pawar_123_y
Contributor II

Thank you for your reply.

I just want to confirm ahab_status command will work on softhsm or not.

Can you please provide me reference document for Softhsm.

0 Kudos
Reply

2,712 Views
b36401
NXP Employee
NXP Employee

You can refer to Code-Signing Tool User's Guide you can get with the bundle of this tool:
http://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL_NEW

0 Kudos
Reply