How to verify real time edge 2.2 function ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to verify real time edge 2.2 function ?

961 Views
t2865k5
Contributor I

Dear NXP,

HW platform : imx8mplus

SW:5.10.72 + Real-time Edge 2.2

(1) I refer to the Real-time Edge Yocto Project User Guide.docx . I build a imx-image-multimedia-imx8mp-lpddr4-evk.wic image (5.10.72 + Real-time Edge 2.2) to download to SD card ,and run command as follows:


stress -i 4 --vm 10 --vm-bytes 10M --vm-hang 100 --timeout 100s
cyclictest --smp -p90 -m

t2865k5_1-1672738198229.png

 

(2) I download  imx-image-multimedia-imx8mpevk.wic (5.10.72) to SD card ,and run command as follows:

stress -i 4 --vm 10 --vm-bytes 10M --vm-hang 100 --timeout 100s
cyclictest --smp -p90 -m

t2865k5_0-1672738177260.png

(3) The actual difference between the two is not big in maximum latency time.

      Could you tell me how to verify real time edge function?

 

 

 

0 Kudos
Reply
1 Reply

949 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the Real-Time Edge Software User Guide chapter 3.1.1 System Real-time Latency tests.

Best regards,
Aldo.

0 Kudos
Reply