Hello,
For the flashing the images, mfg tool is used. How to use the mfg tool for the custom boards?
Regards,
Surendra
Hi Surendra
for new hardware it is necessary to run ddr test and rebuild
mfg tools firmware (files in folder ..OS Firmware/firmware) with new calibration settings found from ddr test
(change them in uboot/board/freescale/../mx6sabresd/*.cfg file), for other hardware changes 
change linux sources and build manufacturing image: bitbake fsl-image-mfgtool-initramfs.
Please use attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have a custom board that I am trying to build the mfgtool firmware required by the manufacturing tool. I am trying to build the fsl-image-mfgtool-initramfs image which depends on u-boot-mfgtool and linux-mfgtool. I get errors related to missing custom board files. How do I integrate my custom board files into the mfgtool build environment?
please check Porting Guide from linux doc package
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS
Best regards
igor
Do not see anything on the manufacturing tool in the Porting Guide.
If you are looking for the flashing the images on the board, few standard tools are available instead of MFG Tool.
Please check following link, it may be useful.
Regards,
Surendra